ON Semiconductor's New Subminiature Package For Voltage Detector Series Promotes Space-Saving Designs

Share

Phoenix, Arizona - August 27, 1999 - Designers can provide voltage continuity for microcontroller systems in about half the space previously used by designing with a new series of voltage detectors introduced by ON Semiconductor, today. Housed in a new subminiature package, the units can be placed anywhere and provide optimal space saving advantages in applications such as laptop computers.

The miniature 4-lead SC-70 (SC-82AB) package measures only 2.0mm x 2.1mm x 0.9mm (length x width x thickness) and is approximately half the size of a SOT-23 package. ON Semiconductor offers two new detectors in the new package, types MC33460 and MC33461, that were designed for use in small, portable, wireless communication applications, where the miniature SC-70 package space saving is very appealing to designers.

These new voltage detectors send a RESET to a MPU/MCU whenever the supply voltage falls below an internally preset threshold. No external components are required, which reduces the overall system cost and complexity while increasing the system reliability. They also have a very wide operating voltage ranging from 0.7V to 10V and feature an ultra low supply current of 0.8 mA typical. The +/- 2% accuracy of the built-in hysteresis ensures stable switching.

The MC33460 features an active low, open-drain RESET output, whereas the MC33461 features an active low, push-pull RESET output. These devices are now available with internally preset thresholds of 0.9V, 2.0V, 2.7V, 2.8V, 3.0V, 3.2V, 4.3V, and 4.5V. Other voltage options can be provided in steps of 0.1V increments.

The MC33460/MC33461 are housed in the new 4-lead SC-70 (SC-82AB) surface mount package. Samples and production quantities are immediately available and are priced at $0.35 each in quantities of 15K units.

About ON Semiconductor
ON Semiconductor, formerly a division of Motorola, is the world's leading supplier of analog, logic and discrete semiconductor components with shipments of 15 billion units in 1998 totaling $1.5 billion in sales. These power and interface products are an integral part of electronics that provide the security, convenience and entertainment in today's world.

Motorola is a registered trademark of Motorola, Inc. Photo available through Editorial contact.

# # #

For more information:

Yinka Massally
Public Relations Manager
ON Semiconductor
602-244-6398

Kent Yancik
Analog Marketing Manager
ON Semiconductor
602-413-6388

Philippe Soum
Analog Marketing Manager
ON Semiconductor
33-5-6119-9726

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.