Breakthrough Power Performance for AI and Electrification

onsemi vertical Gallium Nitride (vGaN) is a breakthrough power semiconductor technology that delivers record efficiency, power density, and ruggedness for the age of AI and electrification. Solving persistent industry challenges such as thermal limitations, power stage efficiency, and bulky system designs. Built using a true GaN-on-GaN vertical architecture, vGaN delivers high-voltage, high-efficiency performance for the rapidly growing power demands of AI data centers, electric vehicles, renewable energy, and aerospace, defense, and security applications.

As power density becomes the currency of competitiveness, onsemi is leading the charge in the future of intelligent power – providing the semiconductor foundation required to scale the next generation of AI infrastructure and electrified systems.

What is onsemi Vertical GaN?

Most GaN is a lateral structure, built on silicon or sapphire. Vertical GaN is GaN built on GaN, where current can run vertically through the chip instead of along the surface. Vertical current enables high power density and higher voltages for far greater performance in a smaller, double-sided cooled package.

The “GaN-on-GaN” architecture, developed through a proprietary process at onsemi fab in Syracuse, NY, is built to deliver on the promise of more efficient, more reliable power systems of the future.

Key Advantages of Vertical GaN

Higher Power Density

Up to 1,200 volts and Beyond.

Efficiency Gains

Reduced energy loss and heat, increasing efficiency by up to 50%.

Compact Designs

Reduced end-system size and weight.

State-of-the-art Manufacturing

66,000 square-foot facility in Syracuse, NY. Proprietary processes grow GaN layers directly on GaN substrates.

Packaging Innovation

Double-sided cooled package.

Future-Proof

vGaN enables switching frequencies much higher than traditional solutions.

Core Technology Applications

AI Data Center

The rapid growth of Artificial Intelligence (AI), cloud and edge computing is driving unprecedented data center expansion. vGaN technology increases power density and reduces power losses and component counts for 800V DC-DC converters – greatly improving cost-per-rack.

View Data Center Solutions

Electric Vehicles

Electrified powertrains are at the heart of sustainable mobility. vGaN technology delivers smaller, lighter and more efficient inverters for increased EV range, enabling robust and scalable designs for Battery Electric Vehicles (BEVs), Plug-in Hybrids (PHEVs) and Mild Hybrids (MHEVs).

View EV Solutions

Renewable Energy

The global transition to electrification is transforming energy infrastructure. With vGaN technology, you get higher voltage handling and reduced energy losses for solar inverters, and fast, efficient, high-density power for energy storage systems.

View Energy Infrastructure Solutions

Aerospace, Defense, and Security

Our solutions enhance situational awareness and decision superiority, extend endurance, and enable advanced capabilities to improve the effectiveness of aerospace, defense and security missions. vGaN brings higher performance, enhanced ruggedness, and more compact designs.

View ADS Solutions

FAQs

View most frequently asked questions about onsemi vGaN technology. 

Today’s commercial GaN devices are typically built in a lateral structure, meaning that GaN is grown on top of a silicon or sapphire substrate. In the case of vertical GaN, GaN is grown on top of a GaN substrate. This vertical design allows current to flow straight through the chip rather than just across its surface, allowing higher current densities and operation at much higher voltages than lateral GaN devices and enabling switching frequencies much higher than silicon or silicon carbide (SiC).

Vertical GaN is called “vertical” because of the way electric current flows through the device. In traditional (lateral) GaN devices, the current moves along the surface of the chip. In contrast, vertical GaN is grown on a GaN substrate, and its unique architecture allows current to flow straight through the chip – from top to bottom – rather than just across its surface. This vertical current flow enables the device to handle much higher voltages and larger currents, resulting in greater power density, higher efficiency, and more compact system designs.

Vertical GaN offers a wider bandgap, higher electron mobility, and higher critical electric field than silicon and SiC. This results in higher switching frequencies, higher breakdown voltages, and superior efficiency. The Baliga Figure of Merit (BFOM) for GaN is approximately 1000 times better than silicon, and defect density is dramatically lower than lateral GaN devices.

onsemi is the first company to bring vertical GaN to market at scale, backed by over 130 patents and a dedicated R&D and manufacturing facility in Syracuse, NY. Its proprietary GaN-on-GaN process delivers unmatched performance, reliability, and efficiency.

Manufacturing vertical GaN requires growing thick, defect-free GaN device layers on bulk GaN substrates—a process far more complex than standard silicon manufacturing. Precise epitaxy and novel fabrication techniques are essential, and even minor crystal defects can impact performance and reliability. onsemi holds over 130 global patents covering all aspects of device architecture and processing.

Vertical GaN (vGaN) is important for the future of AI and electrification because it enables high-efficiency, high-power systems that are critical for managing the growing energy demands of technologies like electric vehicles, renewable energy, and AI data centers.

Vertical GaN enables smaller, lighter, and more efficient power electronics for EVs, including inverters and fast-charging systems. Its high voltage and fast switching capabilities mean EVs can achieve greater driving range, faster charging, and improved reliability, supporting miniaturization of critical automotive components.

AI data centers require high compute density and energy efficiency. Vertical GaN’s superior power density and efficiency reduce energy losses during power conversion, enabling higher performance and lower cooling costs. This allows data centers to pack more computing power into smaller spaces, supporting rapid AI growth while managing energy consumption.

Vertical GaN enables more efficient solar inverters and wind energy conversion systems, maximizing energy capture and reducing losses. Its high voltage capability and ruggedness make it ideal for demanding renewable energy applications.

The technology’s compact size, high reliability, and ability to operate under extreme conditions make it well-suited for aerospace, defense, and security systems requiring rugged, high-performance power electronics.

Support and Updates

If you're interested to learn about any onsemi technology, search for related articles in help library.

Contact GaN Expert

Questions about onsemi GaN solutions? Leave a message.

Support

Variety of ways to contact support for your convenience.

Updates

Stay up to date on GaN and other power solutions from onsemi.