International Microwave Symposium (IMS) – MONTREAL, Canada – June 18, 2012 –

Share

Full front-to-back PDK enables customers of both companies to take full advantage of the industry’s most comprehensive RF and microwave design platform

International Microwave Symposium (IMS) – MONTREAL, Canada – June 18, 2012 – ON Semiconductor Corporation (Nasdaq: ONNN), a premier supplier of high performance silicon solutions for energy efficient electronics, today announced the availability of a full front-to-back process design kit (PDK) for its High-Q™ Integrated Passive Device process. The PDK was developed for use with Agilent Technologies’ Advanced Design System (ADS) 2011 EDA software and enables both ON Semiconductor and Agilent customers to take full advantage of the industry’s most comprehensive RF and microwave design platform.

The High-Q™ IPD process technology from ON Semiconductor offers a copper on high resistivity silicon platform, ideal for the production of passive devices such as baluns, filters, couplers, diplexers and matching networks that are used in portable, wireless and RF applications. IPD technology supports fabrication of copper inductors, precision capacitors, and precision resistors at the company’s world-class 200 mm wafer manufacturing facility located in Gresham, Oregon. IPD provides a cost-effective solution for RF system in package. An economical foundry shuttle service is available for developing engineering prototypes. In addition, ON Semiconductor also offers design services for custom specifications across multiple applications.

"IPD processes have gained significant traction in RF applications and we see a strong interest from our customers for the expanded Agilent ADS platform support,” said Rick Whitcomb, senior director, Custom Foundry and IPD division at ON Semiconductor. "By offering a complete ADS design kit, including layout and integrated EM support, our customers now have the advantage of Agilent's proven expertise in RF and microwave design."

A full feature ADS design kit is available to customers for layout, simulation, and verification that supports schematic-driven layout creation, layout-versus-schematic check and integrated 3D planar electromagnetic and 3D-FEM simulators.

“ADS is a perfect fit for IPD processes and the combination of ADS and ON Semiconductor’s IPD design kit allows our mutual customers access to an effective, integrated design platform,” said Juergen Hartung, foundry program manager of Agilent EEs of EDA. “ADS not only provides a complete front-to-back implementation platform for the IPD die itself, but also directly enables design of the complete RF module in which the IPD is contained.”

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.