ON Semiconductor Introduces Fixed-Frequency Current-Mode Controller for High Efficiency, Compact Adapter Solutions

February 22, 2010

Controllers Offer High Efficiency and Low Standby Power Consumption in Wide Range of AC-DC Adaptor Applications

Fixed-Frequency Current-Mode Controller PhotoAPPLIED POWER ELECTRONICS CONFERENCE (APEC), PALM SPRINGS, Calif. - Booth # 315 – Feb. 22, 2010 – ON Semiconductor (Nasdaq: ONNN) a premier supplier of high performance, energy efficient silicon solutions for green electronics today announced the introduction of  the NCP1237, NCP1238 and NCP1288 fixed-frequency, current-mode controller ICs. Targeted at AC-DC adapter applications for laptop/notebook computers, LCD displays, printers, and household consumer electronics, the new controllers are available in a choice of frequency options with single or dual level over current thresholds. The standard device has a built-in 65 kHz oscillator, with 100 kHz and 133 kHz versions supplied on request.

The proprietary Soft−Skip™ mode utilized by these ICs ramp the peak current gradually during skip mode, reducing the risk of audible noise. This allows additional component savings, along with easing the design and manufacture of the transformer. Combining this with a frequency fold-back function, the new controllers deliver high efficiency levels in light load conditions, while minimizing input power during no load conditions.

The Dynamic Self−Supply (DSS) function of the NCP1237 and NCP1238 provide an integrated start-up current source that intelligently handles start-up and line transient events. This simplifies the design of the auxiliary supply, reducing the size of the VCC capacitor. To minimize external component count, the controllers integrate brown-out, over-power compensation and ramp compensation, allowing a compact solution to be designed.

The new fixed-frequency, current-mode controller ICs have an operational temperature range of −40 °C to +125 °C and are offered in a compact SOIC-7 package.

“With utility bills continuing to increase and concerns about the environment growing, it is vital to use electrical power at the greatest possible rates of efficiency,” said Christophe Warin, AC-DC business unit manager at ON Semiconductor. “The NCP1237, NCP1238 and NCP1288 are highly integrated solutions that will allow engineers to develop power system designs that maintain strong reliability, have a low bill-of-materials and do not waste energy when the product is in standby mode.”

The NCP1237 controller will be featured in a live demo at the ON Semiconductor booth (#315) during APEC, which takes place Feb. 22-25, 2010 in Palm Springs, Calif.

For more information, please visit https://www.onsemi.com.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner and smarter world. onsemi is recognized as a Fortune 500® company and included in the Nasdaq-100 Index® and S&P 500® index. Learn more about onsemi at www.onsemi.com.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.
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
Please select one of the press categories.

Select Language:

Please select at least one of the languages.
Please select at least one of the languages.
Please select at least one of the languages.

*I agree that the information that I provide will be used in accordance with the terms of the onsemi Privacy Policy