ON Semiconductor’s Latest BSI Technology Delivers Best-in-Class Performance for Automotive ADAS and Viewing Cameras

Newest 1/3-inch 1 megapixel backside illuminated (BSI) CMOS image sensor delivers significant improvements in low light signal-to-noise ratio, visible light sensitivity and infrared performance















PHOENIX, Ariz. – July 09, 2015 – ON Semiconductor (Nasdaq: ON), driving energy efficiency innovations, is expanding its highly-regarded 1/3-inch 1 megapixel (MP) image sensor portfolio with early sampling of the company’s first backside illuminated (BSI) sensor technology for the automotive imaging market. The innovative new sensor technology delivers 4x better low light signal-to-noise ratio, a 40 percent increase in visible light sensitivity, and greater than 60 percent improvement in near infrared (NIR) performance than the current market leading AR0132AT CMOS image sensor for advanced driver assistance systems (ADAS).

“The advantages this new BSI technology brings to the automotive market are exciting,” said Sandor Barna, vice president, Automotive and Scanning Division at ON Semiconductor. “The state-of-the-art BSI devices based on this technology, that we currently have in early sampling, exhibit true industry-leading low light performance, and demonstrate our commitment to continued investment in automotive imaging technology.”

The first product to incorporate this new technology will be the AR0136AT 1/3-inch optical format CMOS digital image sensor with 1280 x 960 resolution, and 3.75 micron BSI pixels (p). The AR0136AT supports linear and high dynamic range (HDR) modes, in a single chip HDR solution, with a 120 decibel (dB) dynamic range in HDR mode. It has an output pixel rate of 74.25 MP/second (maximum), which results in a frame rate of 45 frames per second (fps) at 960p resolution and 60 fps at 720p resolution. It has an operating junction temperature range of -40 °C to +125 °C and will be fully qualified to AEC-Q100. Engineering samples will be available in Q3 of 2015, with mass production planned for early 2016.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner and smarter world. onsemi is recognized as a Fortune 500® company and included in the Nasdaq-100 Index® and S&P 500® index. Learn more about onsemi at www.onsemi.com.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.
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
Please select one of the press categories.

Select Language:

Please select at least one of the languages.
Please select at least one of the languages.
Please select at least one of the languages.

*I agree that the information that I provide will be used in accordance with the terms of the onsemi Privacy Policy