ON Semiconductor’s Battery-Free Smart Passive Sensors™ Win China IoT Innovation Award for Outstanding Technical Innovation

SHENZHEN, China. – Dec 5, 2018 –

Share

Comprehensive turnkey solution enables rapid configuration for multi-sensor applications at the network edge

SHENZHEN, China. – Dec 5, 2018 – ON Semiconductor (Nasdaq: ON), driving energy efficient innovations, has been awarded an IoT Outstanding Technical Innovation Award for its Smart Passive Sensors™ (SPS). SPS™ are wireless and battery-free sensors that enable the monitoring of various parameters and, coupled with the company’s SPSDEVK1MT-GEVK turnkey solution kit, enable rapid integration into IoT applications.

SPSDEVK1MT-GEVK is a predictive maintenance turnkey solution kit that integrates 20 SPS1T001PCB temperature sensors, 20 SPSxT001PET temperature sensors, 20 SPSxT001CER temperature sensors, 20 SPSxM001PET moisture sensors, a 12 V universal DC power supply, two UHF antennas (SPSDEVA1-W), and a UHF SPS reader hub (SPSPRDR1-8). Also incorporated is the ON Semiconductor RF TagReader software, which automatically identifies the SPS™ wireless and battery-free sensors to provide a complete solution.

The SPS reader hub provides energy through the UHF antenna, which harvests the sensors to enable to measure and send back highly accurate data rapidly. They allow the monitoring of various parameters such as temperature, moisture and proximity at the network edge where running wires or replacing batteries may be unfeasible. The cost-effective solution has significant benefit to design low-power IoT platforms.

The comprehensive solution composed of sensors with reader system, removing the need to source various IoT solution components from numerous vendors. This speeds up design while reducing cost through the ability to rapidly configure and modify multi-sensor IoT applications. The battery-free feature coupled with the extended reading distance allows the SPS overcoming the limitations of short communication range in NFC technology and eliminating maintenance issue of battery replacement in Bluetooth-based technology.

Organized by elecfans.com, the China IoT Innovation Awards aim to select and recognize innovative technologies with significant impact on the IoT market in China.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.