ON Semiconductor Introduces Industry’s Smallest MOSFETs in Highly Compact, Low Profile Packages

October 16, 2012

Optimized for interface and power management applications in ultra portable consumer electronics

Industry's Smallest MOSGET's for Portable Applications

PHOENIX, Ariz. – Oct. 16, 2012 – ON Semiconductor (Nasdaq: ONNN), a premier supplier of high performance silicon solutions for energy efficient electronics, has expanded on the company’s extensive interface and power management portfolio with the introduction of a pair of ultra small, ultra thin, small signal MOSFETs optimized for space-constrained portable consumer electronics such as tablet computers, smart phones, GPS systems, digital media players and portable games consoles.

“As portable electronics continue to decrease in size while the number of on-board features continue to increase, there is, and will continue to be, an ongoing need for ultra small, high performance components to make feature-rich on-the-go devices energy efficient and highly functioning,” said Paul Leonard, vice president of ON Semiconductor’s MOSFET products division. “The NTNS3193NZ and NTNS3A91PZ do just this by enabling design engineers to specify a device that has the necessary features and functionality while still allowing sleek, stylish designs that consumers have now come to expect.”

The new NTNS3193NZ and NTNS3A91PZ are considered the industry’s most compact small-signal MOSFETs as they are housed in a tiny 0.62 mm x 0.62 mm x 0.4 mm XLLGA3 package. With a total surface mount area of only 0.38 mm², the XLLGA3 package is the ideal solution for the ever shrinking environments of portable electronics, and easily replaces competitive products offered in much bigger packages such as SOT-883 (with a surface mount area of 0.6mm²) or the SOT-723 (with mount area of 1.44mm²).

The NTNS3193NZ is a 20 volt (V), single N−channel, 0.75 ohms typical on resistance at ±4.5 voltage gate to source (VGS) device. This is complemented by the NTNS3A91PZ -20 V, single P−channel device, which has 1.3 ohms typical on resistance at ±4.5 V.

With low RDS(on), low threshold voltage, and 1.5 V gate drive capability, these new MOSFETs greatly reduce power consumption when incorporated in portable electronic products making both devices ideally suited for small signal load switches, analog switches and high speed interfacing. Both devices are fully Pb-free, halogen-free and are RoHS compliant.

Pricing

The NTNS3193NZ and NTNS3A91PZ are priced at $0.33 and $0.35 per unit in 8,000 quantities respectively.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner, and smarter world. onsemi is recognized as a Fortune 500® company and included in the S&P 500® index. Learn more about onsemi at www.onsemi.com.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.