Low Capacitance, Low Clamping Voltage ESD Protection Devices from ON Semiconductor Target Next Generation Interfaces

Transient voltage suppressors optimized for Thunderbolt, USB 3.0/3.1, HDMI 2.0, V-by-One HS and eSATA interfaces















ESD8004 ESD Protection Array.

PHOENIX, Ariz. – April 16, 2014 – ON Semiconductor (Nasdaq: ONNN), driving innovation in energy efficiency, has introduced five new electrostatic discharge (ESD) suppression devices for today’s most advanced interfaces. Patent-pending design techniques and process technology enable these devices to deliver the industry’s lowest capacitance and ESD clamping voltage, suitable for use with extremely high data rate interfaces and small geometry chipsets.

The ESD8000 transient voltage suppressor (TVS) series achieves maximum capacitance specification of 0.35 pF, and ESD clamping voltages down to 8 volts (V) at 16 amperes (A), equivalent to IEC61000-4-2 Level 4 8 kilovolts (kV) contact. The extremely low capacitance nearly eliminates any degradation to the data line signal integrity at data rates greater than 10 Gb/s, supporting emerging interfaces such as USB 3.0, USB 3.1, HDMI 2.0, and Thunderbolt. The low clamping voltage improves protection of system level ESD testing as chipsets evolve into geometries below 20 nanometer (nm), making them more sensitive to transient voltage.

“The innovative technology utilized in these new TVS products resets the boundaries in terms of ESD clamping voltage and delivers ultra-low levels of capacitance,” states Gary Straker, vice president and general manager of ON Semiconductor's Protection Solutions products. “As a result, they can safeguard modern high speed interfaces and integrated circuits based on the latest process technologies from ESD strikes.”

The four-line ESD8004 and ESD8104 can protect two pairs of voltage sensitive high speed data lines in the industry standard footprint of the 2.5 mm x 1 mm UDFN-10 package, making them suitable for the latest serial interface standards such as USB 3.0, HDMI 2.0, and eSATA. The flow-through style package enables easy printed circuit board layout and the matched trace lengths necessary to maintain consistent impedance between high speed differential lines.

The ESD8008 integrates eight lines, or four differential pairs, into a single package for HDMI, DisplayPort, and V-by-One HS interfaces.

The six-line ESD8006 TVS is optimized for protecting the fastest interfaces operating at 10 Gb/s such as Thunderbolt and USB 3.1. These devices have a capacitance of 0.25 pF and utilize single connect flow through routing packages which eliminates the “no connect” pin commonly found on other flow through packages, ensuring minimal parasitic impact to the data line and signal integrity.

The ESD8040 is designed specifically to provide a full function integrated ESD protection device for the HDMI interface and Display Port IOs. This device optimizes pin placement and routing to provide 14 lines of protection required to serve all data, power, and control lines of the interface in an innovative, space saving package that still maintains single connect flow through routing on the high speed lines. The 14 lines of fully integrated protection in a single package, combined with industry leading performance, make this an ideal solution to protect the challenging HDMI 2.0 interface. The ESD8040 is also backwards compatible with HDMI 1.3 and 1.4.

Packaging and Pricing

The ESD8004 and ESD8104 are offered in Pb-free UDFN-10 packages and priced at $0.16 and $0.12 per unit in 3,000 unit quantities, while the ESD8040 is offered in Pb-free UDFN-18 packages and priced at $0.40 per unit in 3,000 unit quantities. The ESD8006 and ESD8008 are offered in Pb-free UDFN-8 and UDFN-14 packages respectively and priced at $0.15 and $0.19 per unit in 3,000 unit quantities.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner, and smarter world. onsemi is recognized as a Fortune 500® company and included in the S&P 500® index. Learn more about onsemi at www.onsemi.com.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.