ON Semiconductor Wins Innovative Automotive Semiconductor Tech Supplier Award

SHANGHAI, China – March 20, 2013

Share

NCV78663 power ballast and dual LED driver for automotive front lighting honored - underlining the company’s innovative technology and continued leadership in automotive electronics















SHANGHAI, China – March 20, 2013 ON Semiconductor Corporation (Nasdaq: ONNN), driving innovation in energy efficiency, has won an "Innovative Automotive Semiconductor Technology Supplier 2012" award for its NCV78663 power ballast and dual LED driver for automotive front lighting applications. The prestigious award is part of Automobil Industrie magazine's program to recognize companies that play an important role in pushing back the boundaries of automotive electronic technology, spanning semiconductor, sensor and connector solutions for the automotive industry.

"We are proud of the recognition that this industry award confers on our automotive product,” said Bob Klosterboer, ON Semiconductor senior vice president and general manager of the Applications Products Group. “This win endorses our R&D process and evidences our leadership as a top 10 global automotive semiconductor supplier. We remain committed to developing innovative and high-performance qualified products and technologies that provide energy efficient automotive solutions to help our customers solve their unique design challenges."

The NCV78663 is a single-chip and high efficient smart power ballast and dual LED driver for advanced LED front lighting systems. Developed to meet system level requirements for driving multiple LED strings of up to 60 volts (V), PWM dimming to maintain LED color temperature, and controlled average current, the NCV78663 enables designers to control high and low beams, daytime running lights, turn indicators, and fog lights with one system-on-chip device. It is a best fit for high current LEDs and provides a complete solution to drive two strings up to 60 V, by means of two internal independent buck switch channels, with a minimum of external components. For each channel, the output current and voltage can be customized according to the application requirements.

Diagnostic functions for automotive front lighting are provided on-chip, and the device also integrates a voltage booster controller, giving designers a unique input current filter with a limited number of externals.

The NCV78663 can be used in stand-alone mode or together with a companion microcontroller, providing maximum flexibility. It can communicate with an external microcontroller to change operating parameters after power-up, implement LED-short detection, and provide advanced system diagnostics.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.