VISION Trade Fair - STUTTGART, Germany – Nov. 4, 2014

Share

New 2.3 megapixel and 5.3 megapixel image sensors combine global shutter with low-noise, high sensitivity and high speed in a hardware scalable solution















VISION Trade Fair - STUTTGART, Germany – Nov. 4, 2014 – ON Semiconductor (Nasdaq: ONNN), driving energy efficiency innovations, has introduced two new higher resolutions CMOS image sensors to its successful PYTHON product family. The new PYTHON 2000 and PYTHON 5000, with resolutions of 2.3 megapixel (MP) and 5.3 MP respectively, address the needs of general purpose industrial image sensing applications such as machine vision, inspection and motion monitoring, as well as security, surveillance and intelligent transportation systems (ITS).

The PYTHON 2000 and PYTHON 5000 have been designed with a focus on performance, versatility and ease of use. Together with the previously released PYTHON 300, 500 and 1300, this entire family of sensors can be supported from a single PCB, greatly simplifying the design of a broad range of cameras offerings. The result is a hardware scalable product family where all sensors have the same data, control and optical interface, thus allowing camera manufacturers to rapidly roll-out products with multiple resolutions, from VGA to 5 MP, with greatly minimized development effort.

“The PYTHON family delivers a high-speed imaging solution without compromising image quality,” said Chris McNiffe, vice president of image sensor products at ON Semiconductor. “A choice of resolutions all supported by a single PCB – plus programmability and numerous features that enhance performance – combine to make the PYTHON family an important addition to the market that will allow designers of industrial image systems to meet the most stringent demands from their customers.”

ON Semiconductor’s patented in-pixel CDS (ipCDS) technology enables global shutter imaging with Correlated Double Sampling (CDS) in a compact pixel size, resulting in CCD-like optical performance in an attractive combination of optical formats and resolutions. The resulting PYTHON pixel allows the capture of fast moving scenes without distortion by combining a read noise of 9 e- with 7.7 V/lux sensitivity and frame rates as high as 850 frames per second (VGA). The devices boast highly attractive speed and optical performance, high configuration flexibility including fast on the fly updates to sensor settings, various trigger and control options, and operational support across the -40°C to +85°C industrial temperature range. Both new sensors are available in mono, color and extended Near-Infrared variants, further expanding PYTHON’s capabilities.

PYTHON 2000 and PYTHON 5000 are sampling today, with full production expected in the first quarter of 2015. For more information about the PYTHON image sensor family, visit www.onsemi.com/python.

VISION Trade Fair

The PYTHON 2000 and PYTHON 5000 Image Sensors will be demonstrated in the ON Semiconductor booth (1C82) at the 2014 VISION trade fair, held November 4 – 6 in Stuttgart, Germany.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.