ON Semiconductor Expands RHYTHM™ Portfolio of Digital Signal Processors for Hearing Aid Market

March 25, 2014

New 16-channel DSP system supports superior sound quality and comfort in high-end designs, while new pre-fit DSP offers common digital features without the need for computer fitting















R3920 Preconfigured DSP System for Hearing Health.

AudiologyNOW! – Orlando, Florida - March 25, 2014 – ON Semiconductor (Nasdaq: ONNN), driving energy efficient innovations, has added two new devices to its RHYTHM™ family of preconfigured Digital Signal Processing (DSP) systems designed specifically for use in hearing aid devices.

RHYTHM R3920 is a 16-channel device that is equipped with advanced algorithms for high-end applications. RHYTHM R3110, meanwhile, brings new features such as noise reduction and feedback cancelation to the entry-level market sector. Both new devices meet the stringent demands of hearing aid designs in all form factors, balancing high performance with energy efficiency.

R3920 supports today’s advanced hearing aids with its feature set and flexibility. The device features 16-channels of wide dynamic range compression (WDRC), providing audiologists the freedom of fine granularity fitting. The iSceneDetect™ environmental classification algorithm on R3920 discerns various sound environments and then selects the most appropriate mode automatically for a high-quality, custom audio experience. Impulse noise reduction, another new feature on R3920, monitors and attenuates sharp, impulsive noises such as clattering dishes that could otherwise be very uncomfortable for hearing aid users. For hearing aid manufacturers, R3920 can use the same shells, schematics and designs as the existing R3910 eight-channel DSP from ON Semiconductor, which can help an existing customer get product to market very quickly and easily.

R3110 brings noise reduction and feedback cancellation to hearing aids in emerging geographies and entry-level markets. R3110 is a turnkey solution that does not require computer fitting or extensive infrastructure, facilitating adoption in these markets. With a pre-fit set of audiology parameters, R3110 eliminates the need for software tools and training, simplifying the deployment process. A number of modes can be configured, such as single or dual-microphone, tinnitus masking, or telecoil.

“I am thrilled about the expansion of our RHYTHM family with two new devices that truly complement our existing portfolio of preconfigured DSPs,” said Michel De Mey, senior director, hearing solutions and consumer health at ON Semiconductor. “These products will provide manufacturers with the ability to address additional markets and meet the specific needs of more hearing aid users.”

The complete portfolio of hearing aid products from ON Semiconductor includes both programmable and preconfigured DSP systems, featuring high-precision sound, ultra-low power consumption, and wireless capability, to address the needs of all hearing aid manufacturers. For more information, visit www.onsemi.com/rhythm.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner, and smarter world. onsemi is recognized as a Fortune 500® company and included in the S&P 500® index. Learn more about onsemi at www.onsemi.com.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.