ON Semiconductor Expands Optical Image Stabilization Portfolio, Bringing Superior Picture Quality to Built-In Camera Applications

February 22, 2016

Advanced optical image stabilization/Auto-focus technologies overcome the performance limitations of traditional camera modules















IOptical Image Stabilization (OIS) / Auto Focus (AF) driver

Mobile World Congress (MWC) – Barcelona, Spain – Feb. 22, 2016 – ON Semiconductor (Nasdaq: ON ),driving energy efficiency innovations, introduces its next generation Optical Image Stabilization (OIS) / Auto Focus (AF) driver, LC898123AXD ,to its portfolio, offering a premier digital still camera and video experience for smart phones, tablets, notebooks, and wearables, by using advanced auto-focus, and optical image stabilization technologies to overcome the performance limitations of traditional camera modules.

The LC898123AXD OIS / AF driver integrates a DSP core with multiple analog peripherals for image stabilization, auto-focus control, and H-bridge and constant-current drivers. The addition of on-chip Flash memory provides storage for the DSP program and calibration parameters, thus saving 90% of the overhead time needed to load from conventional memory on startup. This highly integrated solution enables faster implementation of OIS and AF functionality into camera modules while remaining compatible with a wide array of image sensors. Furthermore, the high level of functional integration supports the need for very thin camera modules.

"There is growing demand for enhanced image clarity and quality in the latest smartphone models, as on-the-go consumers expect to derive better and better user experiences regardless of device size,” said Tomofumi Watanabe, Business Unit Leader of the Power Solutions Products in Intelligent Power Solution Division at ON Semiconductor. “The LC898123AXD enables camera module designers to meet these ever demanding requirements”.

The LC898123 has best-in-class current consumption, enabling improved battery lifetime. The DSP performance and flexibility allows support for various VCM actuators. The high-performance 32-bit DSP optimized for OIS/AF signal processing covers many functions, such as servo control, gyro data filtering, and host command interface. In addition, the LC898123 offers “High Level Command” function to standardize commands from the main CPU to the camera module, enabling phone developers to use standardized commands for multiple camera modules/actuators without changing CPU software.

Reference designs dedicated to Camera Module Integrators are available, accelerating the OIS/AF evaluation as well as reduce the development workload.

Packaging and Pricing
The LC898123AXD is offered in a Pb-free WLCSP-35 package and is priced at $ 2.18 per unit in 4,000 unit quantities.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner, and smarter world. onsemi is recognized as a Fortune 500® company and included in the S&P 500® index. Learn more about onsemi at www.onsemi.com.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.