ON Semiconductor Expands its High Performance Trench Field Stop IGBT Portfolio for Motor Control, Solar and Uninterruptable Power Supply Applications

October 22, 2012

New field stop trench technology devices expand current ratings and deliver high speed switching capabilities for demanding power applications.

High Performance 1200 V Trench Field Stop IGBT

PHOENIX, Ariz. – Oct. 22, 2012 – ON Semiconductor (Nasdaq: ONNN), a premier supplier of high performance silicon solutions for energy efficient electronics, has expanded its NGBTxx family of 1200 volt (V) trench field stop (FS) insulated gate bipolar transistor (IGBT) devices with nine new energy efficient solutions.

The new devices improve overall system switching efficiency, lower power dissipation and improve system reliability. Adding to the company's existing family of over thirty IGBTs, the newest devices expand the available product ratings up to 40 A. This includes devices specifically targeted at high performance power conversion in solar power and uninterruptable power supply (UPS) implementations.

“Dramatic increases in global energy consumption and projected unfavorable environmental and economic impacts continue to drive demand for higher performance power discrete components,” said John Trice, senior director and general manager for ON Semiconductor’s Power Discrete products. “This new generation of devices brings cost-effective, industry-leading power efficiency without sacrificing robustness. With ON Semiconductor’s proprietary Trench Field Stop Technology, we can now give engineers a greater breadth of options to choose from when implementing their power system designs.”

The first group of new IGBTs are the NGTB40N120FLWG, NGTB25N120FLWG and NGTB15N120FLWG. These products feature a robust and cost effective trench technology construction, and provide superior performance in high frequency switching applications.. Low switch losses and an ultra fast recovery diode make them ideal for high frequency solar, UPS and inverter welder applications. The devices have IC rating of 40 A, 25 A and 15 A respectively. All three devices are highly optimized for switching applications with frequencies from 10 kilohertz (kHz) to 40 kHz, delivering low on-state voltage (VCEsat) and low gate charge (Qg) characteristics, as well as exhibiting ultra-fast recovery and minimal switching losses to keep power dissipation low. These new IGBT devices all have an operational junction temperature range of −55 °C to +150 °C.

The second new group of devices also broaden the portfolio of Trench FS IGBT devices by increasing product ratings up to 40 A. The NGTB30N120LWG and NGTB40N120LWG offer low Vcesat and rugged short circuit characteristics with fast recovery diodes for low frequency (2 – 20 kHz) hard switching applications, such as motor control inverters applications. Complementing these devices are the NGTB30N120IHLWG, NGTB40N120IHLWG, NGTB20N120IHSWG, and NGTB30N120IHSWG, which feature balanced switching and conduction losses for induction heating and other soft switching applications operating at medium frequencies (15 – 30 kHz) including hot pots, rice cookers and microwave appliances.

Packaging and Pricing

The NGTB15N120FLWG, NGTB25N120FLWG, NGTB40N120FLWG, NGTB30N120IHLWG, NGTB40N120IHLWG, NGTB30N120LWG, NGTB40N120LWG, NGTB30N120IHSWG, NGTB20N120IHSWG, and are all offered in compact Pb−free TO−247 packages. They are respectively priced at $2.00, $2.50, $4.00, $2.50, $2.75, $3.00, $3.25, $2.25, $1.60 unit in 10,000 unit quantities.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner, and smarter world. onsemi is recognized as a Fortune 500® company and included in the S&P 500® index. Learn more about onsemi at www.onsemi.com.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.