ON Semiconductor Expands Breadth of Options for Low-Light Industrial Imaging Applications

September 20, 2016

New 8-megapixel IT-EMCCD device, integrated cooler option for family provide new capabilities for medical, scientific & surveillance imaging

PHOENIX, AZ – Sept. 20, 2016 – ON Semiconductor (Nasdaq: ON ), driving energy efficient innovations, continues to strengthen its position in low-light imaging solutions for industrial markets with the introduction of new products based on interline transfer electron multiplying charge-coupled device (IT-EMCCD) technology.

The new 8-megapixel KAE-08151 image sensor is the second device to use the company’s IT EMCCD technology, delivering the same sub-electron noise floor and imaging versatility as the existing 1080p resolution KAE-02150 image sensor. With a 22 millimeter diagonal (4/3 optical format) that matches the imaging path of professional microscopes, the KAE-08151 directly targets high resolution microscopy and scientific imaging applications operating in lighting regimes that can range from sub-lux to bright-light imaging. In addition, a new packaging option is available for both devices in this family which incorporates a thermoelectric cooler (TEC) directly into the package design. This integrated cooler simplifies development of a cooled camera that optimizes the performance available from these devices.

“The compelling combination of performance and flexibility provided by IT EMCCD technology is providing significant benefits for low-light imaging across key industrial imaging applications,” stated Herb Erhardt, Vice President and General Manager, Industrial Solutions Division, Image Sensor Group at ON Semiconductor. “By expanding our product portfolio with a new resolution node and options that simplify the integration process for camera manufacturers, end customers will be presented with even more ways to leverage the advantages of this unique technology.”

IT EMCCD devices combine two established imaging technologies with a unique output structure to enable a new class of low-noise, high-dynamic range imaging. While interline transfer CCDs combine superior image quality and uniformity with a highly efficient electronic shutter, this technology is not always ideal for very low-light imaging because of the overall noise floor of their outputs. Conversely, EMCCD image sensors excel at low-noise imaging, but historically have been available only as low resolution devices with limited dynamic range. Combining these technologies allows the low-noise architecture of EMCCD to be extended to multi-megapixel resolution image sensors for the first time, and an innovative output design allows both standard CCD (low-gain) and EMCCD (high-gain) outputs to be utilized for a single image capture – extending scene detection from sunlight to starlight in a single image.

The KAE-08151 is sampling today in Monochrome and Bayer Color configurations in a CPGA-155 package, with samples incorporating an integrated TEC available in the first quarter of 2017. The KAE-02150, already in production, is now sampling in a CPGA-143 package that incorporates an integrated TEC. All package options are RoHS-compliant. Both devices will be demonstrated in ON Semiconductor’s booth (1C32) at the 2016 VISION trade fair, held November 8-10 in Stuttgart, Germany.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner, and smarter world. onsemi is recognized as a Fortune 500® company and included in the S&P 500® index. Learn more about onsemi at www.onsemi.com.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.