ON Semiconductor CCD Image Sensor Delivers Enhanced Performance for Intelligent Traffic, Surveillance, Medical Imaging and Industrial Inspection

New KAI-08051 8 megapixel image sensor leverages technology acquired with Truesense Imaging to provide improved light sensitivity and reduced read noise















KAI-08051 CCD Image Sensor.

PHOENIX, AZ. - July 14, 2014 – ON Semiconductor (Nasdaq: ONNN), driving energy efficient innovations, is enhancing the charge-coupled device (CCD) image sensor portfolio recently acquired from Truesense Imaging with new technology that improves imaging performance for industrial applications.

The new KAI-08051 Image Sensor provides improved light sensitivity, reduced read noise, and improved color accuracy compared to the previous generation device, expanding opportunities for 8 megapixel image capture in demanding imaging applications such as Intelligent Traffic, Surveillance, Medical Imaging, and Industrial Inspection.

“CCD image sensors continue to provide the critical image quality required in many key applications,” said Chris McNiffe, Vice President, Image Sensor Business unit at ON Semiconductor. “The enhanced performance available from the new KAI-08051 Image Sensor reflects our on-going commitment to improve the capability of our existing products and to deliver the industry’s most advanced image sensors using both CCD and CMOS technology.

The KAI-08051 Image Sensor shares the same advanced 5.5 micron pixel architecture, 8 megapixel resolution, 15 frame per second readout rate, and 4/3 optical format as the existing KAI-08050 Image Sensor, but improves key performance parameters through the use of an improved amplifier design, newly optimized microlens structure, and new color filter pigments in both Bayer and Sparse color configurations. The KAI-08051 is backward compatible with the KAI-08050, requiring at most minor modifications to the firmware used in existing camera designs. This allows the new image sensor to retain “Plug-and-Play” interoperability with the full family of 5.5-micron Interline Transfer CCD devices, enabling a single camera design to support image sensors ranging in resolution from 1 to 29 megapixels.

The KAI-08051 Image Sensor is now in production and is available in Monochrome, Bayer Color, and Sparse Color configurations. An evaluation kit is available that allows the imaging performance of this new device to be quickly and easily examined in detail without the need to develop a full camera design.

For technical questions, please contact ON Semiconductor at (585) 784 5500 or info@truesenseimaging.com. Visit our blog at www.onsemi.com/blog.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner, and smarter world. onsemi is recognized as a Fortune 500® company and included in the S&P 500® index. Learn more about onsemi at www.onsemi.com.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.