SHENZHEN, China – May 28, 2014 –

Share

The company’s 1,200 volt and 1,350 volt Field Stop II IGBTs honoured as Best Power Supply Devices















SHENZHEN, China – May 28, 2014 – ON Semiconductor (Nasdaq: ONNN), driving energy efficient innovations, has won the Best Power Device Award at Electronic Engineering & Product World (EEPW)'s 2013 Power Supply Products Award. Run annually by one of China's leading semiconductor industry media titles, the award program recognizes excellence in power supply components in six different categories.

ON Semiconductor's high performance Field Stop II (FSII) IGBT portfolio expands current ratings and delivers efficient, high-speed switching capabilities for power applications such as uninterrupted power systems (UPS), hot pots, rice cookers and microwaves. The winning devices, the NGTBxxN120IHRWG and NGTBxxN135IHRW, feature optimized switching and reduced conduction losses for induction heating and soft switching applications operating at medium frequencies of 15 kilohertz (kHz)-30 kHz. With excellent ruggedness and superior on-state characteristics at high currents, these devices are optimized based on system requirements to enable higher efficiency and lower system losses.

Further expansion of the FSII IGBT technology includes the NGTBxxN120FL2WG and NGTBxxN135FL2WG family of devices designed specifically for solar inverter, UPS, and inverter welder applications. With improved thermal characteristics, these devices will have an operational junction temperature range of -55°C to +175°C and increase in current ratings up to 100 amperes (A) in TO-247 packages.

ON Semiconductor has already established a reputation for the quality and reliability of its IGBTs, with automotive AEC-Q qualified IGBT’s in production for more than a decade. In 2011, the company started new development work on high-voltage/high-current devices for a range of industrial and consumer marketing applications, which continue to demand high-efficiency solutions. The first full portfolio family of the company’s proprietary Trench Field Stop technology was released in 2012, matching competing technology. The launch of this award-winning FSII IGBT product family in May 2013 reinforced the company's status as a technology leader – a status that has now been recognized by the votes of EEPW readers and the decision of the judging panel.

The annual EEPW Power Supply Products Award program, now in its eleventh year, is open to embedded system suppliers worldwide. The publication presents Best Product and Best Application awards in six product categories. Products are selected from a host of competing products through a combination of online voting and the decision of a judging panel of industry experts appointed by EEPW.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.