ON Semiconductor Unveils New Micro-Packaged ESD Protection Diodes and Schottky Diodes for Portable and Wireless Applications

Share

New SOD-923 package provides a 38 percent reduction in footprint over existing packaging and delivers the industry’s lowest forward voltage

PHOENIX, Ariz. – Sept. 19, 2006 - ON Semiconductor (Nasdaq: ONNN), a leading global supplier of efficient power management solutions, has introduced three new ESD diodes and three Schottky diodes in an ultra small SOD-923 package. The package measures a mere 1.0 mm x 0.6 mm with a 0.4 mm profile yet delivers impressive performance. These diodes are ideal for portable, consumer and wireless products requiring efficient power and best in class ESD protection using minimal board space.

“ON Semiconductor is an industry leader in micro packaging and strongly committed to providing smaller and smaller high-performance package options for space-constrained portable applications,” said Mamoon Rashid, general manager of ON Semiconductor’s Discrete Product Group. “Our newest package – the SOD-923 – delivers better overall performance than competitive devices. Until now, an SOD-723 with a 0.084 mm2 footprint was the smallest package ON Semiconductor offered for these ESD and Schottky devices. Our new SOD-923 package delivers a 38 percent reduction in footprint for handheld applications where board space saving is critical, without a corresponding reduction in performance.”

ESD Protection Diodes
The ESD9X3.3S, ESD9X5.0S and ESD9X12S are designed to clamp fast-rising ESD pulses to prevent damage to voltage sensitive components on the board. These devices provide the highest level of ESD protection available in the SOD-923 package as measured by the IEC61000-4-2 ESD compliance standard. Their small size facilitates placement near input/output ports where ESD can enter the system. As such, the devices suppress the transient voltage before it can be coupled into the rest of the board. The ESD9X series of diodes feature lower clamping voltage and lower leakage than multi-layer varistors of comparable size.

Budgetary pricing for these devices is $0.034 USD per unit for quantities of 10,000 units.

Schottky Barrier Diodes
The NSR0130P, NSR0230P, and NSR0140P are Schottky barrier diodes designed for high-speed switching applications and use in discrete boost and buck conversion. Featuring extremely low forward voltage (Vf) to reduce conduction losses, these new Schottky’s are more efficient than integrated solution alternatives. The devices provide true design flexibility and power savings by creating a direct current (dc) supply at voltages not already available from a given power management unit (PMU). Additionally, the flexibility inherent in these Schottky’s helps designers incorporate expanded features that require diverse voltage requirements. Such features could include camera, camera flash and LED backlighting.

Budgetary pricing for these new Schottky diodes is $0.034 USD per unit for quantities of 10,000 units.

For additional information about all the ESD protection diodes and Schottky diodes offered by ON Semiconductor, visit https://www.onsemi.com or contact Lon Robinson at Lon.Robinson@onsemi.com.

About ON Semiconductor
With its global logistics network and strong portfolio of power semiconductor devices, ON Semiconductor (Nasdaq: ONNN) is a preferred supplier of power solutions to engineers, purchasing professionals, distributors and contract manufacturers in the computer, cell phone, portable devices, automotive and industrial markets. For more information, please visit ON Semiconductor’s website at https://www.onsemi.com.

# # #

ON Semiconductor and the ON Semiconductor logo are registered trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the company references its website in this news release, such information on the website is not to be incorporated herein.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.