ON Semiconductor Unveils Innovative Modular Automotive Imaging Platform

Autonomous Vehicles - SANTA CLARA, Cal. – Feb. 27, 2017

Share

Complete ecosystem in a compact form-factor enables accelerated time-to-market & significant reductions in allocated engineering resources

Autonomous Vehicles - SANTA CLARA, Cal. – Feb. 27, 2017 – ON Semiconductor (NASDAQ: ON), driving energy efficient innovations, has introduced the Modular Automotive Reference System (MARS) that gives system and software developers a ready-to-use camera for research and development activities. The leading-edge MARS platform enables users to reconfigure cameras with different lenses, image sensors, image signal processors (ISPs) and communications options for rapid prototyping and experimentation. The system is so flexible that it can be used for the full spectrum of automotive camera applications including advanced driver assistance systems (ADAS), surround and rear viewing systems, in-cabin cameras (for gesture recognition, driver eye monitoring, or light level inspection purposes), and autonomous driving.

MARS enables shorter design cycles, reduced engineering costs, and assists automotive design teams in the implementation of imaging systems by providing them with a unique mix-and-match solution. Through it, various items of hardware can be combined in a robust and highly adaptable system with a compact form-factor. Due to the many different boards available, engineers have access to ON Semiconductor’s broad portfolio of image sensors and co-processors, plus various automotive communications protocols from a select group of third party supply partners. This provides extensive scope in terms of finding the combination that best fits specific system requirements. The versatile platform can accommodate an almost limitless number of combinations due to consistent signal/power definitions for the interconnects utilized by these respective boards.

The ease of adapting this modular solution means that undertaking time-consuming activities such as creating custom boards (each capable of accommodating a different sensor option), testing out high-speed interface standards, or writing code for drivers, is no longer necessary. MARS is supported by a complete ecosystem, encompassing software development tools, schematics, gerbers, bill-of-materials (BOM) and much more. A comprehensive user guide is also included within the accompanying documentation.

“As image sensing proliferates in automotive applications, MARS will provide system and software developers tasked with turning concepts into reliable working applications with a valuable platform to simplify and speed proof of concept and development, and offer the scalability to get ideas from the lab to on-vehicle testing in real-world conditions,” said Ross Jatou, General Manager and Vice President of Automotive Solutions Division of Image Sensor Group at ON Semiconductor. “The flexibility of MARS accelerates the component selection process by making the constituent sensors and co-processors totally interchangeable. The platform avoids the need to construct a multitude of custom boards to house different sensors for evaluation reducing engineering effort and shortening project times.”

The support of commonly used communication standards (such as GMSL, FPD-Link, LVDS, MIPI, Ethernet) enables direct interfacing with existing vehicle electronic control units (ECUs). ON Semiconductor is working with an ecosystem of partners spanning lens developers, third party ISP vendors, communications IC vendors, software developers and SoC vendors. MARS modules are already prequalified with a range of these third party products and the company will expand these offerings going forward.

Availability
MARS development boards are available now. The MARS product recommendation tool provides a convenient, step by step process to select the correct board(s) for your design. Watch the Introduction to MARS webcast, read the blog, “Optimizing the Automotive Camera Development Phase Using a Modular Design Approach”, and visit the website for more detailed information. Board pricing is available on request and enables fully configured cameras at $1,000.00 or less.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.