ON Semiconductor to Demonstrate Innovative Intelligent Sensing Solutions for Industrial Applications at Vision China

SHANGHAI, China – July 1, 2020 -

Share

Company to exhibit imaging technologies for applications ranging from high resolution inspection and machine vision to industrial artificial intelligence

SHANGHAI, China – July 1, 2020 - ON Semiconductor (Nasdaq: ON)), driving energy efficient innovations, will demonstrate its wide range of intelligent image sensing solutions at Vision China 2020 to be held July 3-5 in Shanghai.

Exhibits will include a global shutter image sensor for high resolution inspection, an X-Cube reference design for industrial camera design, and an artificial intelligence (AI) demonstrator for machine vision using the AR1335 image sensor, A 4K resolution super high dynamic range (HDR) sensor for machine vision will also be featured alongside the AR0234 digital image sensor with global shutter for scanner and intelligent transportation system (ITS).

ON Semiconductor will demonstrate the excellent imaging sensitivity and versatility of a 45 megapixel (MP) running at up to 60 frame per second (fps) in 8K video mode while providing state of the art image quality in 12 bit mode image sensor for high-resolution inspection for smart factory applications.

The X-Cube reference design based on the X-class image sensor family provides 16 MP resolution in a 1.1 inch optical format to supply the imaging detail and performance needed for 29 mm x 29 mm industrial camera foot print for machine vision and ITS. The reference design is a complete system solution incorporating a C-mount lens holder, FPGA conversation from HiSPi to MIPI output, and interface to Demo3 and DevWare ecosystem.

An innovative AI demonstrator for machine vision using the AR1335 sensor in a system that is trained to recognize and classify the quality and condition of fresh and rotted fruits will show-case how to develop and integrate AI into systems and products for machine vision.

ON Semiconductor will also demonstrate solutions for outdoor applications. A 4K resolution sensor with up to 4-exposure HDR-on-chip is ideal for ultra-high-definition image capture in high-end surveillance systems. The XGS family includes ITS optimized products with resolutions ranging from 3 MP up to 12 MP to support traffic management under the most demanding conditions. The AR0234 captures high quality, accurate and fast-moving scenes with a 2 MP global shutter at 120 fps to provide clear, low noise images in both low−light and bright scenes for ITS and scanner applications.

For a first-hand exploration of these innovative sensing solutions, visit the ON Semiconductor booth (D225) in Hall 7.1 at Vision China, July 3-5 in Shanghai.

Also, ON Semiconductor experts will address two imaging seminars on July 3. The two presentations are:
1. The Challenges for Image Sensors in Industrial AI Applications to be presented at 10:30 in Hall 7.1 on the trade show floor
2. LiDAR Applications to be presented at 14:00 in meeting room M703, close to Hall 7.1

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.