PHOENIX, Arizona – 4, September, 2019 –

Share

Compliance with IEEE 802.3bt delivers 90 Watts of power to applications including smart sensors, building automation and connected lighting

PHOENIX, Arizona – 4, September, 2019 – ON Semiconductor (Nasdaq: ON), driving energy efficient innovations, is leading the industry with its support for the IEEE 802.3bt standard, thanks to a growing portfolio of compliant products and technologies. Using the new IEEE 802.3bt standard, Power over Ethernet (PoE) can be used to deliver high-speed connectivity up to 90 W of power over Local Area Network (LAN) connections. ON Semiconductor’s solutions not only support the new standard power limit, but extends it further to 100 W for systems including telecommunications and digital signage.

The new IEEE 802.3bt standard for PoE has the potential to transform every vertical market touched by the IoT, by enabling more sophisticated endpoints operating across larger networks. The IEEE 802.3bt standard optimizes energy management through the new “Autoclass” feature, which enables Powered Devices (PDs) to communicate their specific power needs to the Power Sourcing Equipment (PSE). This in turn allows each PSE to allocate just the right amount of power to each PD, maximizing both the available energy and bandwidth.

With up to 90 W of power available, compared to the 30 W provided by the IEEE 802.at standard (PoE+), IEEE 802.3bt can provide both power and connectivity to new applications that would otherwise require a dedicated and typically off-line power source. PoE will simplify network topologies and provide a more robust ‘plug and play’ user experience.

“Power over Ethernet is one of the fastest-growing markets for power semiconductors today, with a compound average unit growth rate of 14% expected from 2017 through 2022,” said Kevin Anderson, senior analyst, power semiconductors at business information provider IHS Markit. “The additional power-delivery capability defined in IEEE 802.3bt enables new applications, such as higher-powered connected lighting, networked high-resolution surveillance cameras and high-performance wireless access points.”

Forming the foundation of ON Semiconductor’s PoE-PD solutions, the NCP1095 and NCP1096 Interface Controllers incorporate all of the features needed to implement a PoE interface, including detection, auto-classification and current limiting. The controllers employ either an external (NCP1095) or internal (NCP1096) hot-swap FET. The integrated hot-swap FET in the NCP1096 features the lowest on-resistance available in a Type 3 or Type 4 PoE controller. The controllers are complemented by the NCP1566 DC-DC Controller, the FDMC8622 Single MOSFET and the FDMQ8203 and FDMQ8205A GreenBridge™ Quad MOSFETs, which have been developed to provide a more efficient alternative to a diode bridge in PoE applications. Together, these devices enable highly efficient PoE interfaces with up to the standard limit of 90 Watts of power or to a proprietary 100 W solution if more power is needed.

“As a company focused on energy efficiency, we are really excited to help PoE achieve its full potential,” commented Ryan Cameron, Vice President of Industrial and Off-Line Power Solutions at ON Semiconductor. “By providing a complete family of IEEE 802.3bt compliant solutions, we have made the technology more accessible for all development engineers which will help enable many more connected devices with guaranteed interoperability.”

For more information, contact your local ON Semiconductor representative or authorized distributor.

Additional resources & documents:

Landing page:Power over Ethernet (PoE) Solutions

Video:You Need More Power


Blog:Opening the Door for Higher Power IoT Applications

White paper: Quad MOSFET Approach Delivers Dramatic PoE Efficiency Improvements over Diode Bridge Alternatives

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.