ON Semiconductor Offers Integrated Switching Regulators to Enable High Efficiency Offline Power Converters for Consumer Applications

Integrated 650 volt avalanche-rated MOSFETs enable robust, compact switching solutions for power-hungry applications such as household appliances, DVD players and set top boxes















High voltage switching regulator for Offline SMPS.

PHOENIX, Ariz. – July 28, 2014 – ON Semiconductor (Nasdaq: ONNN), driving energy efficient innovations, has added three new current mode, fixed frequency switching regulators to its expansive power management product portfolio. Targeted at use in compact, high reliability offline AC-DC switched-mode power supplies, the NCP1129, NCP1126, and NCP1124 incorporate an avalanche-rated 650 volt (V) MOSFET and frequency foldback along with skip mode that improve the light load and standby efficiency, meeting the ENERGY STAR® EPS 2.0 Standard.

The high degree of integration results in minimal external components and significantly reduces the overall bill of materials, making them highly suited to power system designs for household appliances, DVD players and set top boxes. The NCP1129, NCP1126, and NCP1124 can deliver up to 25 W, 15 W and 12 W respectively and each generate a jittered 65 kilo Hertz (kHz) or 100 kHz switching frequency, resulting in marked improvements in electro-magnetic interference (EMI) performance.

“This new NCP112x series of switchers enable power system design engineers to create more energy efficient and more cost effective power supply designs that will fit into confined spaces,” said Shane Chilton, senior director, AC-DC Power Conversion Products at ON Semiconductor. “The design flexibility provided by specifying these devices allows engineers to optimize their design implementations for either heightened power efficiency or reduced board real estate.”

It is possible for the maximum peak current to be adjusted via an external resistor, facilitating ramp compensation, so that stable continuous conduction mode (CCM) operation can be maintained. The frequency foldback mode permits power conversion efficiency levels to be raised under light load conditions, while the skip mode can be activated for reducing standby power consumption at (or close to) a no load scenario - with less than 100 milliwatts (mW) drawn at high line when in standby mode.

The NCP112x devices all have a wide array of protective features including a 50 ms timer-based auto-recovery short-circuit protection function. Furthermore, short-circuit fault conditions can be independently detected from the auxiliary winding voltage, thereby ensuring that comprehensive safeguards against short-circuit occurrences are in place. The devices incorporate built-in thermal shutdown and over-voltage response mechanisms, as well as a 2 kilovolt (kV) human body model (HBM) resilience rating to electrostatic discharge. An operational temperature range of -40 °C to +150 °C is supported.

Packaging and Pricing

The NCP112x integrated switching regulators are offered in Pb-free PDIP-7 packages, with pricing starting at $0.32 per unit in 10,000 unit quantities.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner and smarter world. onsemi is recognized as a Fortune 500® company and included in the Nasdaq-100 Index® and S&P 500® index. Learn more about onsemi at www.onsemi.com.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.
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
Please select one of the press categories.

Select Language:

Please select at least one of the languages.
Please select at least one of the languages.
Please select at least one of the languages.

*I agree that the information that I provide will be used in accordance with the terms of the onsemi Privacy Policy