ON Semiconductor Moves to New Level of Precision Analog with Ultra-Low-Power, High-Accuracy Analog Voltage Reference ICs

Phoenix, Ariz. – August 10, 2009 -

Share

CAT8900 devices offer accuracy as high as 0.02 percent with low, 800 nA maximum supply current for precision performance in test equipment and portable systems

CAT8900 family of high-accuracy voltage reference integrated circuits (ICs) Phoenix, Ariz. – August 10, 2009 - ON Semiconductor (Nasdaq: ONNN), a leading global supplier of high performance, energy efficient, silicon solutions has moved to a new level of cost-effective, precision analog with its new CAT8900 family of high-accuracy voltage reference integrated circuits (ICs).  The CAT8900 family combines very high initial accuracy, low supply current consumption and a stable temperature coefficient, to enable precision performance in test equipment and portable, battery-powered data acquisition systems. 

The CAT8900 ICs provide a highly accurate voltage reference, with initial accuracy as high as 0.02 percent [± 0.5 millivolts (mV)] and a stable, 20 parts per million per degrees Celsius (ppm/ºC) temperature coefficient, while maintaining a low maximum supply current consumption of 800 nanoamperes (nA).  The low current consumption allows the CAT8900 voltage references to remain powered on continuously, with minimal battery load.  The low power consumption, combined with the very high initial accuracy and temperature stability of the devices, makes them ideal replacements for power-hungry, higher cost bandgap references in a wide range of portable applications. These include handheld medical devices, high resolution A/D (analog-to-digital) and D/A (digital-to-analog) converters, and precision regulator systems.

The CAT8900 family offers nine voltage reference choices:  1.024 volts (V), 1.200 V, 1.250 V, 1.800 V, 2.048 V, 2.500 V, 2.600 V, 3.000 V and 3.300 V.  Custom voltages are available on request.  Each reference is available in four accuracy grades:  ±0.5 mV, ±1.0 mV, ±2.5 mV and ±5.0 mV.  The devices source or sink up to 10 milliamps (mA) of load current with as little as 50 mV of dropout. In most applications they do not require an output bypass capacitor. 

Packaging and Pricing
The CAT8900 precision voltage references come in a Pb-free, RoHS-compliant, 3-lead SOT-23 package.  The per unit prices for quantities of 10,000 are:  $0.60 USD for ±5.0 mV initial accuracy versions; $0.92 USD for ±2.5 mV initial accuracy versions; $1.55 USD for ±1.0 mV initial accuracy versions ; and $2.44 USD for ±0.5 mV initial accuracy versions.  Samples are available now.  Projected lead-time for production quantities is currently eight to 12 weeks after receipt of order (ARO).

About ON Semiconductor
With its global logistics network and strong product portfolio, ON Semiconductor (Nasdaq: ONNN - News) is a preferred supplier of high performance, energy efficient, silicon solutions to customers in the power supply, automotive, communication, computer, consumer, medical, industrial, mobile phone, and military/aerospace markets. The company's broad portfolio includes power, analog, DSP, mixed-signal, advance logic, clock management, non-volatile memory and standard component devices. The company operates a network of manufacturing facilities, sales offices and design centers in key markets throughout North America, Europe, and the Asia Pacific regions. For more information, visit https://www.onsemi.com

#  #  #

ON Semiconductor and the ON Semiconductor logo are registered trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the company references its Web site in this news release, such information on the Web site is not to be incorporated herein.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.