ON Semiconductor launches World’s First Automotive Qualified SiPM Array Product for LiDAR Applications

March 01, 2021

PHOENIX, Ariz. – March 1, 2021 – ON Semiconductor (Nasdaq: ON), driving energy efficient innovations, today announced the new RDM-Series silicon photomultiplier (SiPM) array that extends the LiDAR sensor capabilities to its broad portfolio of intelligent sensing solutions. The ArrayRDM-0112A20-QFN is the first automotive qualified SiPM product in the market, ready for the growing demands in LiDAR applications for the automotive industry and beyond.

The ArrayRDM-0112A20-QFN is a monolithic 1×12 array of SiPM pixels based on the company’s market−leading RDM process, which enables high sensitivity to near-infrared (NIR) light to achieve industry-leading 18.5% photon detection efficiency (PDE)¹ at 905 nanometers (nm). The high internal gain of the SiPM allows sensitivity down to the single-photon level, a feature that in combination with the high PDE, enables the detection of the faintest return signals. This results in the ability to range to greater distances even with low reflective targets.

SiPM technology has gained momentum in recent years and has become the sensor of choice for broad-market depth sensing applications due to its unique feature set. SiPMs have the ability to deliver the highest signal-to-noise performance for long distance ranging in bright sunlight conditions. Additional benefits including lower supply biases and lower sensitivity to temperature changes make it an ideal upgrade for systems that use legacy avalanche photodiodes (APDs). SiPMs are produced in a high-volume CMOS process, allowing for the lowest detector cost and therefore enabling broad-market LiDAR solutions.

Using laser light to measure the distance of an object has spanned the fields of automotive, consumer and industrial applications. In automotive, LiDAR can be employed to improve safety and driver assistance systems (ADAS), aiding features such as lane keeping and traffic jam assist by complementing and providing redundancy with other sensing modalities. LiDAR is becoming commonly used for fully autonomous driving use cases, such as robotic transportation, to safely navigate the environment in real time. Benefiting from the high PDE of ArrayRDM-0112A20-QFN, LiDAR systems supporting these functions have been proven to range over 300 meters in distance. More distance gives more time for the vehicle to respond to unexpected obstacles.

“The high-resolution depth data provided by LiDAR enables instantaneous and accurate object identification in challenging low light conditions. As the first automotive qualified SiPM, the ArrayRDM-0112A20-QFN will enable long range, cost-effective LiDAR solutions for the next level of safety and autonomy,” commented Wade Appelman, senior director, Automotive Sensing Division at ON Semiconductor. “We are continuously enhancing our sensor portfolio by offering diverse and complementary sensing modalities that pave the way to higher levels of ADAS and autonomous driving.”

“At Yole Développement (Yole), we see LiDAR as a critical component on the route to full autonomy in automotive, with functionality required to reach level 2+ and above. Producing sensors that pass automotive qualification, and with a sufficient level of performance, will be a key enabler to the mass adoption of LiDAR for automotive applications, which, based on current trends, is expected to show a +144% CAGR between 2019 and 2025²,” explained Pierrick Boulay, Technology & Market Analyst at Yole.

The ArrayRDM-0112A20-QFN is AEC-Q102 qualified and developed in accordance with IATF 16949. For more information regarding our LiDAR solutions, please contact a local sales office.

Additional resources:

¹ Max PDE at typical operating voltage and 21°C. PDE increases to >25% at 905 nm at elevated temperature.

² Source: LiDAR for Automotive and Industrial Applications 2020 report, Yole Développement (Yole), 2020

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner, and smarter world. onsemi is recognized as a Fortune 500® company and included in the S&P 500® index. Learn more about onsemi at www.onsemi.com.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.