ON Semiconductor Introduces Series of Boost Regulators with a Wide Range of Input Voltages for Battery Powered Applications

Share

NCP144x devices deliver up to 33 percent more output current than competitive devices, offer low standby current and enable both low cost power conversion and significant design flexibility

PHOENIX, Ariz. – Nov. 24, 2003 - Continuing to expand its presence in the portable and wireless markets, Semiconductor (Nasdaq: ONNN) today introduced the NCP144x series of 280 kilohertz (kHz) and 560 kHz boost regulators offering design engineers low cost power conversion solutions for a wide range of battery operated applications.

Each of the four new current mode boost regulators features a 4 Amp (A) / 40 volt (V) integrated power switch that eliminates the need for an external FET - thus saving both cost and board space. The flexibility of the design allows the parts to operate in most power supply configurations, including boost, flyback, forward, inverting and SEPIC. Because the devices operate at voltages ranging from 2.7 V to 30 V, they accommodate numerous applications including test equipment, handheld meters, portable printers and computers, and process control.

Complete News Release

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.