Share

NUS3116 reduces required board space for small form factor portable electronics

PHOENIX, Ariz. – July 27, 2007 – ON Semiconductor (Nasdaq: ONNN), a global supplier of efficient power management solutions, today introduced the NUS3116, an integrated charging and power switching circuit for small form factor portable electronics like cellular phones. This circuit combines a main battery switch, wall charging switch, and USB charging switch elements into a single component, optimizing charging performance and saving critical space on circuit boards in handheld electronic devices.

The NUS3116 is an integration of main power switch, −12 volt (V), −6.2 amps (A), μCool™ single P−channel MOSFET to handle the main battery switch function and two internal low saturation PNP transistors to handle dual channel charging elements. With 40 mili ohm (m) maximum RDS(ON), the main switch MOSFET minimizes power loss during battery operation of portable electronics. The dual low-Vce(sat) transistors provide good thermal performance for charge currents up to 2 A, and have a Vce voltage drop of less than 240 mili volts (mV) at the end of the charging.

Offered in a DFN-8 package that requires only 9 mm2 of board space, the NUS3116 provides a board savings of more then 20 mm2 versus typical solutions using three TSOP-6 packages with interconnect space. The package’s low profile of 0.8 mm allows the device to be used in small form factor designs. Use of the NUS3116 integrated device also reduces the complexity of circuit board layout.

The NUS3116 is available in a Pb-free DFN-8 package, and is priced at $0.80 per unit in 3000 unit quantities.

For additional information, visit www.onsemi.com or contact Sam.Abdeh@onsemi.com.

About ON Semiconductor
With its global logistics network and strong portfolio of power semiconductor devices, ON Semiconductor (Nasdaq: ONNN) is a preferred supplier of power solutions to engineers, purchasing professionals, distributors and contract manufacturers in the power supply, computer, consumer, portable/wireless, automotive and industrial markets. For more information, please visit ON Semiconductor’s website at https://www.onsemi.com.

# # #

ON Semiconductor and the ON Semiconductor logo are registered trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the company references its Web site in this news release, such information on the Web site is not to be incorporated herein.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.