ON Semiconductor Introduces New Dual Output White LED Drivers for LCD Display Backlighting - Housed in the Industry’s Smallest Package

Share

NCP5602 and NCP5612 charge pump white LED drivers feature programmable dimming, achieve 87 percent peak efficiency and deliver consistent brightness for handheld and consumer applications

CPS Expo 2006– Shanghi, China - Nov. 1, 2006 - ON Semiconductor (Nasdaq: ONNN), a leading global supplier of efficient power management solutions, expands its LED portfolio with the addition of two dual output white LED drivers for handheld and consumer applications. Offered in the tiny 2.0 mm x 2.0 mm x 0.55 mm LLGA-12 package, the NCP5602 and NCP5612 are the industry’s smallest dual output charge pumps for driving LCD display backlighting. Each device achieves up to 87 percent peak efficiency with 0.2 percent LED-to-LED matching, thus assuring matched and consistent brightness.

The NCP5602 and NCP5612 have a built-in ICON function that drives a low current through one of the two LEDs, allowing the clock display to be seen even in a dark environment. This dimming mode eliminates the need for additional software programming and simplifies overall design. To ensure safe operation without adding extra components, the NCP5602 and NCP5612 feature short-circuit and overvoltage protection. Complete release

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.