Share

Drawing only 22 microamps of standby current, the NCV8664 provides increased design flexibility to meet tight quiescent current targets

CONVERGENCE – DETROIT, Mich. – October 16, 2006 - ON Semiconductor (Nasdaq: ONNN), a global leader in power management products, today introduced the NCV8664 – the industry’s first linear regulator to incorporate reverse battery, short circuit and overload protection with the lowest quiescent (Iq) current performance specified over a wide automotive temperature range.

An increased number of on-board automotive system power modules need to meet stringent requirements for ignition-off current. Many of these modules have specified currents of less than 100 microamps (μA) of current. Power optimization in the new NCV8664 enables designers to minimize the quiescent current for the regulation portion of the module, allowing higher system level design for controller-area networks (CAN or LIN), microprocessors, and other system overhead.

The NCV8664 is a low drop out (LDO) regulator with a precision 5 volt (V) fixed output and an output current capability of 150 milliamps (mA). Optimized for use in automotive electronics modules requiring tight quiescent currents, the NCV8664 draws only 22 μA typical and 30 μA maximum of quiescent current specified from -40C to 85C. This is a wider temperature range than most low Iq regulators on the market. The output voltage of the LDO is accurate to within ±2.0 percent. The device is also internally protected against input supply reversal, output overcurrent faults, and excess die temperature.

“As electronics have become more pervasive in automobiles, lowering the quiescent current of each power module to minimize overall battery drain has become increasingly important,” said Andy Williams, ON Semiconductor senior vice president and general manager of the Automotive and Power Regulation Division. “ON Semiconductor is committed to developing and delivering versatile, high performance solutions, such as the NCV8664, to help designers meet these ongoing power system challenges. During the next few quarters, ON Semiconductor plans to further expand its portfolio of low quiescent current regulators to provide additional family members.”

Packaging and Price
The NCV8664DT50RKG is available in a Pb-free DPAK and priced at $1.00 per unit in 2,500 unit quantities. The NCV8664ST50T3G is available in a Pb-free SOT-223, priced at $1.00 per unit in 4,000 unit quantities.

For additional technical information visit www.onsemi.com or contact Christel Moreau at christel.moreau@onsemi.com.

About ON Semiconductor
With its global logistics network and strong portfolio of power semiconductor devices, ON Semiconductor (Nasdaq: ONNN) is a preferred supplier of power solutions to engineers, purchasing professionals, distributors and contract manufacturers in the computer, cell phone, portable devices, automotive and industrial markets. For more information, please visit ON Semiconductor’s website at https://www.onsemi.com.

# # #

ON Semiconductor and the ON Semiconductor logo are registered trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the company references its Web site in this news release, such information on the Web site is not to be incorporated herein.<.i>

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.