ON Semiconductor Introduces Intelligent Power Modules that Integrate Pre-Driver and Output Stage with Bootstrap and Protection Functions

Portfolio Includes 10 A, 15 A, and 20 A Devices for White Goods and Industrial Motor Applications















STK551U3A2AE Intelligent Power Module.

PHOENIX, Ariz. – March 11, 2014 - >– ON Semiconductor (Nasdaq: ONNN), driving energy efficient innovations, has introduced seven highly integrated three-phase intelligent power modules (IPM) for motor controls in white goods and industrial applications. The highly integrated hybrid device portfolio contains all of the power stage functions, including pre-driver and output stage power devices with boot strap diodes, under-voltage protection, and over-current protection.

The IPMs are composed of power devices and gate drivers with 600 volts (V) maximum voltage, and the maximum operating voltage for the inverter units is 450 V. STK544UC62K-E, STK551U362A-E, STK554U362A-E, and STK554U362C-E deliver maximum output current of 10 amperes (A); STK551U392A-E and STK554U392A-E deliver maximum output current of 15 A; and STK551U3A2A-E delivers maximum output current of 20 A.

These IPMs can operate at a switching frequency up to 20 kilohertz (kHz). Insulated Metal Substrate Technology (IMST®) from ON Semiconductor enables the IPMs to deliver high power efficiency with low noise. The high integration levels of the devices themselves, combined with the smaller external components, enable the power system control boards to be physically smaller, with fewer components, fewer high voltage circuit board traces, and less complicated assembly.

“In the white goods market, power efficiency continues to be a priority,” said Chris Chey, general manager of the IPM division of ON Semiconductor. “The integration level of these Intelligent Power Modules helps our customers increase efficiency and reduce noise in white goods control circuits, while reducing design time.”

The GreenPoint® online analysis tool from ON Semiconductor provides an interactive environment to analyze IPM performance. Users can select the device to analyze, set operating conditions, view performance simulations, and download results.

Packaging and Pricing

The STK544UC62K-E is offered in Pb-free SIP-23 packages. The STK551U362A-E, STK554U362A-E, STK554U362C-E, STK551U392A-E, STK554U392A-E, and STK551U3A2A-E are offered in Pb-free SIP-29 packages. Budgetary pricing ranges from $6.00 to $8.40 per unit.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner, and smarter world. onsemi is recognized as a Fortune 500® company and included in the S&P 500® index. Learn more about onsemi at www.onsemi.com.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.