ON Semiconductor Introduces Industry’s First Floating, Regulated Charge Pump to Replace Isolated Power Supplies

Share

The new NIS6201 provides a regulated output voltage – allowing it to ‘float’ this bias or supply voltage on top of any bus voltage making it applicable to a wide range of applications

Phoenix, Arizona October 31, 2005 – A global supplier of advanced power management solutions, ON Semiconductor (Nasdaq: ONNN) today introduced the NIS6201 – the industry’s only floating regulated charge pump for low power applications. Designed to supply 20 milliamp (mA) and 8 volt (V) to 15 V, the NIS6201 is an extremely cost-effective replacement for a small, isolated, switching power supply. Ideal applications for the device include the drive voltage for ORing Diodes, floating supervisory circuits and LED drivers.

Whereas most charge pumps typically have their output voltage referenced to ground, the NIS6201 output voltage can be referenced (or added to) any bus voltage. This allows it to ‘float’ a bias or supply voltage on top of any bus voltage. This device enables designers to easily generate any bias voltage with minimal external components.

The NIS6201 contains an internal linear regulator and a versatile charge pump that allow bias voltage supplies to be transferred from a ground referenced source to a higher potential. Because the high voltage components are external to the pump and can be sized accordingly, the NIS6201 can handle any isolation voltage required - up to hundreds of volts. The device also features an adjustable voltage output and is thermally protected. Using the NIS6201, designers can easily create a bias voltage with few external components and no inductor – thus saving size, weight and cost.

“The NIS6201 is a big step forward in designing economical ‘housekeeping’ supplies – or the auxiliary supplies needed to provide power to the main PWM control IC or to power ICs for functions that aren’t always on,” said Sue Nee, marketing manager of Application Specific Integrated Products at ON Semiconductor. “If an additional output voltage is required late in a design cycle, the NIS6201 can be a quick and easy solution.”

Features
• Integrated Linear Regulator and Charge Pump
• Thermal Limit Protection
• Adjustable Voltage Output
• High Voltage Isolation

Applications
• ORing Diodes
• Floating Supervisory Circuits
• LED Driver

Packaging and Price
The NIS6201 is offered in a lead free, SO-8 package and priced at $0.53 per unit in 10,000 unit quantities. Samples and a demo board are available. For additional technical information visit https://www.onsemi.com/tech or contact Sue Nee at Sue.Nee@onsemi.com.

About ON Semiconductor
With its global logistics network and strong portfolio of power semiconductor devices, ON Semiconductor (Nasdaq: ONNN) is a preferred supplier of power solutions to engineers, purchasing professionals, distributors and contract manufacturers in the computer, cell phone, portable devices, automotive and industrial markets. For more information, please visit ON Semiconductor’s website at https://www.onsemi.com.

# # #

ON Semiconductor and the ON Semiconductor logo are registered trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the company references its website in this news release, such information on the website is not to be incorporated herein.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.