ON Semiconductor Introduces High Performance Field Stop IGBTs for High Efficiency Power Conversion

May 08, 2012

New 1200 volt devices offer optimal solution for high power inductive heating and inverter applications

Field Stop IGBTs for High Efficiency Power Conversion

Power Conversion Intelligent Motion (PCIM), NUREMBERG, Germany – May 8, 2012 – ON Semiconductor (Nasdaq: ONNN), a premier supplier of high performance silicon solutions for energy efficient electronics, today introduced a new series of Field Stop Insulated Gate Bipolar Transistors (IGBTs) targeted at industrial motor control and consumer products. The NGTB15N120, NGTB20N120 and NGTB25N120 enable high performance power conversion solutions for a wide range of demanding applications, including induction cook tops, rice cookers and other small kitchen appliances.

Increasing energy prices and environmental concerns around carbon emissions are continuously driving demand for higher performance power discrete components; especially in high power inductive and inverter applications. These new 1200 volt (V) rated IGBTs utilize deep trench technology and state-of-the-art wafer thinning and processing techniques to enable very low turn-off losses while maintaining a low "ON" state voltage during turn-on, which results in lower switching and conduction losses. These devices are offered with a choice of 15 ampere (A), 20 A and 25 A current ratings and are co-packaged with a very low forward drop and soft-recovery fast rectifier to meet stringent customer requirements for high efficiency while providing a space efficient complete solution.

"ON Semiconductor has been a market leader in delivering high performance and reliable IGBTs to the automotive segment for more than a decade," said John Trice, senior director and general manager for ON Semiconductor's Power Discrete Division. "The new 1200 V series of high performance IGBTs leverages our intellectual property and competencies in high voltage trench and wafer processing technologies while providing customers in a broad range of market sectors with a high quality and robust solution for their demanding power applications".

Packaging & Pricing
The TO-247 packaged Field Stop IGBT devices save board space and are optimized for very low on-state voltage drop and turn-off switching losses. The NGTB15N120IHLWG, NGTB20N120IHLWG, and NGTB25N120IHLWG inductive heating specific IGBTs are priced at $1.50, $1.80, and $2.00 per unit respectively, all in quantities of 2,500. The NGTB15N120LWG, NGTB20N120LWG, and NGTB25N120LWG motor drive specific IGBTs are priced at $1.75, $2.10, and $2.35 respectively, all in quantities of 2,500.

PCIM - ON Semiconductor Booth - Hall 12, Stand No. 371
ON Semiconductor will be featuring live product presentations for 8 –10 at Stand #371 in Hall 12 of the Exhibition Centre Nuremberg.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner, and smarter world. onsemi is recognized as a Fortune 500® company and included in the S&P 500® index. Learn more about onsemi at www.onsemi.com.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.