Share

The new NCP5810 is an efficient and integrated solution that generates both positive and negative output voltage and offers best-in-class performance in a low profile package

PHOENIX, Ariz. – June 7, 2007 - ON Semiconductor (Nasdaq: ONNN), a global leader in power semiconductor solutions, has introduced the NCP5810– a 2 watt (W) dual output dc-dc converter that offers both positive and negative output. The device’s output voltage accuracy, high switching frequency, and small package size makes it particularly suitable for powering a display driver in Active Matrix Organic Light Emitting Diodes (Active Matrix OLED or AMOLED) panel, an emerging display technology for portable applications.

“The NCP5810 presents great advantages for the AMOLED power supply,” said Manor Narayanan, vice president and general manager of ON Semiconductor’s Digital and Consumer Products Group. “ON Semiconductor is dedicated to working with customers to design devices that meet their specific needs. A successful example of such collaboration is the NCP5810, which has been selected by the leading display manufacturer to power the new AMOLED panel for ultra thin portable multimedia devices and is already in mass production.”

Active Matrix OLED – the latest display technology, where only a handful of display manufacturers will be ready to go mass production later this year or next year – delivers better color contrast and video playback quality than today’s LCD displays but creates added power management challenges for design engineers. For example, because AMOLED displays are sensitive to changes in power supply voltages, ON Semiconductor designed the NCP5810 to provide accurate feedback voltage with 1 percent tolerance and a fast line transient response with overshoot of 4 millivolt (mV), given a 500 mV input voltage variation.

Featuring high overall efficiency up to 85 percent at 1.75 megahertz (MHz) oscillator frequency, the NCP5810 dual output dc-dc converter delivers best-in-class performance. In order to complement the slim form factor of AMOLED display, the converter switches at the high 1.75 MHz frequency, allowing the use of small inductors and ceramic capacitors. Its ultra-thin package with 0.55 mm thickness allows the NCP5810 to fit into the thinnest portable design form factor. In addition, it preserves battery power in shut-down mode with true cut-off function that limits the leakage display current to typically 1 microamp (µA). Additionally, the NCP5810 features cycle-by-cycle peak current limit and thermal shut down protection.

Packaging and Pricing

Available in the ultra-thin 3.0 mm x 3.0 mm x 0.55 mm LLGA-12 package, the NCP5810 is budgetary priced at $1.20 USD per unit in 3,000 unit quantities.

In addition to the NCP5810 with fixed converter output voltage, ON Semiconductor is sampling the adjustable version NCP5810A, offered in the same package.

For additional technical information visit www.onsemi.com, or contact Crystal Lam at Crystal.Lam@onsemi.com.

About ON Semiconductor

With its global logistics network and strong portfolio of power semiconductor devices, ON Semiconductor (Nasdaq: ONNN) is a preferred supplier of power solutions to engineers, purchasing professionals, distributors and contract manufacturers in the power supply, computer, consumer, portable/wireless, automotive and industrial markets. For more information, please visit ON Semiconductor’s website at https://www.onsemi.com

# # #

ON Semiconductor and the ON Semiconductor logo are registered trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the company references its website in this news release, such information on the website is not to be incorporated herein.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.