ON Semiconductor introduces Digital Image Sensor with Class-Leading Low Light Sensitivity and Signal-Noise Ratio

Highly sensitive CMOS sensor is optimized for extreme low light and high contrast image capture

PHOENIX, Ariz. – 10 April, 2018 – ON Semiconductor (Nasdaq: ON), driving energy efficient innovations, has introduced the industry’s first 1/1.7-inch 2.1 megapixel CMOS image sensor featuring ON Semiconductor’s newly developed 4.2μm Back Side Illuminated (BSI) pixels – the AR0221 delivers class-leading low light sensitivity for industrial applications.

The AR0221 offers exceptional 3-exposure line-interleaved High Dynamic Range (HDR) with a sensor resolution of 1936H x 1096V, supporting frame rates of 1080p at 30 fps and an outstanding Signal-Noise Ratio (SNR) across visible and near-infrared wavelengths. Its 16:9 ratio with vivid colors and high contrast make it ideal for demanding industrial applications.

Gianluca Colli, Vice President and General Manager, Consumer Solution Division of Image Sensor Group at ON Semiconductor said: “The AR0221 represents the industry’s best CMOS image sensor in this class, thanks to its outstanding low light sensitivity and SNR performance. By including features like windowing, auto black level correction and an onboard temperature sensor, ON Semiconductor has produced an image sensor that will enable a new generation of security and surveillance cameras.”

The sensor offers dual data interfaces in the form of 4-lane MIPI CSI-2 and HiSPi SLVS. Designed to meet industrial-grade specifications, the AR0221 can operate in harsh outdoor environments where operating temperatures can range between -30°C and+85°C. Packaged in a durable, reliable and robust iBGA package with anti-reflection coating on its cover glass, the AR0221 is programmable through a simple two-wire serial interface.

The AR0221 is in production and available now in 12mm x 9mm iBGA package in RGB Bayer color.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner and smarter world. onsemi is recognized as a Fortune 500® company and included in the Nasdaq-100 Index® and S&P 500® index. Learn more about onsemi at www.onsemi.com.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.
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
Please select one of the press categories.

Select Language:

Please select at least one of the languages.
Please select at least one of the languages.
Please select at least one of the languages.

*I agree that the information that I provide will be used in accordance with the terms of the onsemi Privacy Policy