ON Semiconductor Introduces a New Integrated Voltage Regulator that Offers a Low-Power Solution for Battery Powered Applications

50 mA Low Drop Out Linear Voltage Regulator offers high ripple rejection, excellent noise performance and a fast turn on time.

NCP508 image - a low current voltage regulatorPHOENIX, Ariz. – March 31, 2010 – ON Semiconductor (Nasdaq: ONNN), a premier supplier of high performance, energy efficient silicon solutions for green electronics, today introduced the NCP508 – a low current voltage regulator that offers an efficient and economical solution to generating a low power voltage rail. The new regulator provides a solution that supports low power, space efficient and cost-effective designs in applications such as touch screens, keypads, smart phones, portable meters, printers and remote controls.

The NCP508 can drive currents in excess of 50 mA and is housed in a compact SC-88A package with a footprint measuring 2.2 mm x 2.2 mm with an overall height of 1.10 mm. The new device offers high ripple rejection of 70 dB typical (at 1 kHz) that makes it an effective filter for voltage supplies.  Excellent noise performance of 40 µVrms (at 1.5 V) contributes to a very clean output voltage, and when disabled a current consumption of less than 1 µA helps to further extend battery life in portable equipment. Low voltage dropout performance of 140 mV at 30 mA load provides flexibility in designing auxiliary power rails. A switch on time of less than 20 µs is significantly faster than most competing products and allows designers to maximize energy savings by powering down the device when the functionality it supports is not in use. The NCP508 can be used with low-cost ceramic capacitors, further enhancing its appeal as an economical voltage regulator solution.

The NCP508 has a maximum operating voltage of 7 V, though it can withstand high voltage transients of up to 13 V, thus saving cost by alleviating the need for external protection circuitry. Standard output voltage versions of 1.5 V, 1.8 V, 2.5 V, 2.8 V, and 3.3 V are offered with other voltage values available in 100 mV steps. Each device incorporates both current limit and over temperature protection circuits. The operating temperature range is -40 °C to +85 °C.

“These new voltage regulation solutions offer a cost-effective alternative to discrete components that also use more board space and consume more power,” said Mike Paquette, director of the Regulation products at ON Semiconductor. “The NCP508 meets all the requirements involved in the design and development of small, battery powered products that need an economical, robust, reliable and easy-to-use voltage regulation solution with minimal power consumption.”

Pricing and Availability

Offered in an SC-88A package, the NCP508 is budgetary priced at $0.20 per unit for quantities of 3,000 units. A 1.5mm x 1.5mm DFN option is expected to be available later this year.

For more information, please visit https://www.onsemi.com.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner, and smarter world. onsemi is recognized as a Fortune 500® company and included in the S&P 500® index. Learn more about onsemi at www.onsemi.com.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.

If you are a member of the press and are interested in receiving onsemi press releases via email, please complete the form below.

* Full Name

* Email

* Media you represent

* Press Category

*Required fields

Choose your prefered language. You can choose more than one.