ON Semiconductor Expands PureEdgeTM Silicon-Based Crystal Oscillator Clock Module Portfolio

PHOENIX, Ariz. – April 27, 2011 –

Share

NBX series new product additions enable dual voltage capabilities, new frequencies with total frequency stability as low as ±20 ppm to keep pace with increased complexity demanded by next-generation systems

PHOENIX, Ariz. – April 27, 2011 – ON Semiconductor (Nasdaq: ONNN) a premier supplier of high performance, energy efficient silicon solutions, today announced the further extension of its silicon based crystal oscillator (XO) clock module range. The six new additions to the NBX series provide a cost-effective, high accuracy reference clock solution with dual voltage capabilities and class-leading total frequency stability as low as ±20 parts per million (ppm). The new devices meet clock generation requirements in the latest 2.5 V / 3.3 V low-voltage positive emitter coupled logic (LVPECL) designs for applications in routers, switches, servers, and basestations.

The new devices support frequencies for applications such as SONET, Gigabit Ethernet, and LAN/WLAN.  The NBX series offers equivalent or better performance compared to quartz-based third overtone XOs or surface acoustic wave (SAW) products. This is underlined by ultra-low phase noise of -160 decibels relative to the carrier per hertz (dBc/Hz), typical RMS phase jitter of 0.5 picoseconds (ps), and a low bit error rate.

“This frequency and voltage range expansion gives designers of LVPECL clock tree designs even greater choice,” said Ryan Cameron, director, custom industrial and timing products business unit at ON Semiconductor. “With improved performance, dual voltage flexibility and reduced lead times compared to quartz-based alternatives, the NBX series is keeping ahead of the increasing demands of applications in this sector.”

New frequencies supported are 622.08 megahertz (MHz) for the NBXMBB024 and NBXSBB024; 156.25 MHz for the NBXHGA017; 125.00 MHz for the NBXHGA019; 161.1328 MHz for the NBXSGA008; and 50.00 MHz for the NBXHGA053.

Pricing and Availability
The NBX devices are packaged in Pb-free, RoHS compliant, hermetically sealed 5.0 mm x 7.0 mm x 1.9 mm ceramic CLCC-6 SMD packages.  Budgetary pricing for these products is $3.00-$5.50 per unit for quantities of 1,000 units.

For more information, please visit https://www.onsemi.com.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.