New dual or single input MOSFET/ IGBT drivers are pin-to-pin compatible with industry standards

PHOENIX, Ariz. – April 3, 2008 - ON Semiconductor (Nasdaq: ONNN), a global leader in efficient power solutions, has expanded its MOSFET driver integrated circuit (IC) portfolio with the introduction of four new devices - the NCP5106, NCP5104, NCP5111 and NCP5304. These new power gate drivers target low- to mid-power applications and can be used in end products such as white goods, lighting ballasts, and industrial applications such as motor control.

These new high voltage, high-side and low-side drivers are specified over a wide temperature range -40 degrees Celsius (°C) < TJ < 125 °C, and can operate with an input voltage up to 600 volts (V), easing time and effort of design. All the devices feature a dV/dt immunity of 50 volts per nanosecond (V/ns) and are 3.3 V and 5 V input logic compatible. These devices use the bootstrap technique to ensure a proper drive of the high-side power switch and provide rugged design.

The NCP5104, NCP5106B, NCP5111, NCP5304 are high voltage power gate drivers that provide two outputs for direct drive of two N-channel power MOSFETs or IGBTs arranged in a half-bridge configuration. The NCP5106A can be used in any other high-side plus low-side configuration.

Offered in both SOIC-8 and PDIP-8 packages, and priced respectively at $0.80 and $0.96 per unit in 2,500 unit quantities, the NCP5104, NCP5106, NCP5111and NCP5304 are pin-to-pin compatible with industry standard devices.

For additional technical information visit www.onsemi.com, or contact Christophe Warin at Christophe.Warin@onsemi.com.

About ON Semiconductor
With its global logistics network and strong product portfolio, ON Semiconductor (Nasdaq: ONNN) is a preferred supplier of efficient power solutions to customers in the power supply, automotive, communication, computer, consumer, medical, industrial, mobile phone, and military/aerospace markets. The company’s broad portfolio includes power, analog, DSP, mixed-signal, advance logic, clock management and standard component devices. Global corporate headquarters are located in Phoenix, Arizona. The company operates a network of manufacturing facilities, sales offices and design centers in key markets throughout North America, Europe, and the Asia Pacific regions. In March, 2008, ON Semiconductor acquired AMI Semiconductor and all products formerly owned by AMIS. For more information, visit https://www.onsemi.com.

# # #

ON Semiconductor and the ON Semiconductor logo are registered trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the company references its Web site in this news release, such information on the Web site is not to be incorporated herein.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.