ON Semiconductor Expands Power Factor Controller Portfolio with Four New Complementary Devices

Share

Power Factor Correction (PFC) controllers enable the development of highly-efficient power supplies that help designers meet emerging global efficiency standards

INTERNATIONAL IC China (IIC) - SHENZHEN, China – March 5, 2007 - ON Semiconductor (Nasdaq: ONNN), a leading global supplier of efficient power management solutions, today announced the expansion of its industry-leading portfolio of Power Factor Correction (PFC) controllers. Designed for use in lighting, adapters, ATX supplies, flat-panel TVs and other power applications, the four new devices enable the development of highly-efficient power supplies that meet emerging global energy efficiency and power factor standards.

“The introduction of these devices extends ON Semiconductor’s leadership position in power factor controllers,” said Andy Williams, senior vice president and general manager of the Automotive and Power Regulation Group. “The four new devices complement our existing PFC product portfolio by providing industry standard replacements with improved features, new and innovative control methods, and added functions that ease both the time and effort required to design highly efficient Switch Mode Power Supplies. To address our customers’ ongoing demand for ever more efficient power management, we will continue to develop PFC solutions targeted to meet their design challenges.”

The Devices
The NCP1605 is an enhanced, high voltage and efficient standby mode power factor controller that can work in fixed frequency Discontinuous Conduction Mode (DCM) or/and in Critical conduction Mode (CRM). The device incorporates all the features necessary for building robust PFC stages. The NCP1605 can operate as a PFC master, ensuring that a power supply’s second stage only starts up under safe conditions. In addition, it integrates the skip cycle capability to minimize stand-by losses. Offered in a Pb-free SOIC-16 package, the NCP1605 is budgetary priced at $1.07 USD per unit in 1000 unit quantities.

The NCP1606 series are CRM power factor controllers specifically designed for use as a pre-converter in electronic ballast, ac adapters, flat TVs and other low to mid power off-line converters, typical up to 300 watts (W). These devices incorporate adjustable over voltage protection, and built-in under-voltage protection. The NCP1606A and NCP1606B provide a pin-to-pin compatible replacement for industry standard devices. The NCP1606B further reduces power losses by proposing a lower over voltage protection current and a lower current sense threshold. The devices are offered in a Pb-free SOIC-8 package, budgetary priced at $0.335 USD per unit in 2500 unit quantities. They are also available in a Pb-free PDIP-8 package, budgetary priced at $0.405 USD per unit in 1000 unit quantities.

The NCP1654 and NCP1655 are Continuous Conduction Mode power factor correction controllers. They control the power switch conduction time in a fixed frequency mode and in dependence on the instantaneous coil current. They also integrate high safety protection features like a brown-out function, an effective input power runaway clamping circuitry, and minimize the number of external components required for circuit implementation. The NCP1654 is pin-to-pin compatible with industry standard devices, while the NCP1655 offers a pin-to-pin upgrade to ON Semiconductor’s popular NCP1653 fixed-frequency current-mode PFC controller. The new devices are offered in a Pb-free SOIC-8 package, budgetary priced at $0.80 USD per unit in 2500 unit quantities. They are also available in a Pb-free PDIP-8 package, budgetary priced at $0.88 USD per unit in 1000 unit quantities.

For additional technical information or to order samples, visit https://www.onsemi.com or contact Christophe Warin at Christophe.Warin@onsemi.com.

About ON Semiconductor
With its global logistics network and strong portfolio of power semiconductor devices, ON Semiconductor (Nasdaq: ONNN) is a preferred supplier of power solutions to engineers, purchasing professionals, distributors and contract manufacturers in the power supply, computer, consumer, portable/wireless, automotive and industrial markets. For more information, please visit ON Semiconductor’s website at https://www.onsemi.com.

# # #

ON Semiconductor and the ON Semiconductor logo are registered trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the company references its website in this news release, such information on the website is not to be incorporated herein.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.