ON Semiconductor Expands High Performance Clock Management Portfolio with Low Skew Fanout Buffers

Share

New functions and increased performance levels offer better timing accuracy for high performance telecom, networking and ATE applications

PHOENIX, Ariz. – Jan. 8, 2007 -Expanding its high performance portfolio of clock management solutions, ON Semiconductor (Nasdaq: ONNN) has introduced three new highly accurate, low skew, 1:4 clock fanout buffers with CMOS outputs. The NB3N551, NB3L553, and NB3N2304NZ significantly outperform competitive devices. Used to create multiple copies of clocks at full system frequencies, the new devices are ideal for use in telecommunications, networking and automated test equipment (ATE).

“With a portfolio that encompasses clock synthesis, clock generation and clock distribution, ON Semiconductor is quickly emerging as a key player in the market space,” said Bill Hall, ON Semiconductor senior vice president and general manager of the Standard Products Group. “Our competitively priced timing solutions deliver the industry’s highest performance and best quality. The company’s reputation for solid delivery and superior customer service serves to further strengthen the confidence of our customers. During the coming year, we plan to introduce additional high performance clock solutions that target the demanding technological needs of the telecom and data communications marketplace.”

The Devices
The NB3N551 clock fanout buffer operates at up to 180 megahertz (MHz), and at VCC of 3.3 volts (V) or 5.0 V. The device provides an upgrade to the industry standard ICS551, with improved maximum output skew of 160 picoseconds (ps) versus 250 ps for existing products. Packaged in a lead free (Pb-free) SOIC-8 package or a space-saving (2.0 mm x 2.0 mm) DFN-8 package, the NB3N551 is budgetary priced at $0.80 USD per unit in 2,500 unit quantities.

The NB3L553 clock fanout buffer operates at up to 200 MHz with only 35 ps typical skew between outputs and is pin compatible to the industry standard ICS553. The device operates at VCC of 2.5 V, 3.3 V or 5.0 V. It is packaged in the Pb-free SOIC-8 and budgetary priced at $0.87 USD per unit in 2,500 unit quantities.

Operating at up to 140 MHz with a maximum skew of 100ps, the NB3N2304NZ clock fanout buffer is a pin compatible second source to the industry standard ICS2304NZ. This device operates at VCC of 3.0 V to 3.6 V and is ideal for PCI/PCI-X applications. Packaged in a 4.4 mm x 3.0 mm Pb-free 8-pin TSSOP, the NB3N2304NZ is budgetary priced at $0.87 USD per unit in 2,500 unit quantities.

For additional technical information or to order samples, visit https://www.onsemi.com or contact Prescott Sakai at Prescott.Sakai@onsemi.com or Joe Staszkow at Joe.Staszkow@onsemi.com

About ON Semiconductor
With its global logistics network and strong portfolio of power semiconductor devices, ON Semiconductor (Nasdaq: ONNN) is a preferred supplier of power solutions to engineers, purchasing professionals, distributors and contract manufacturers in the computer, cell phone, portable devices, automotive and industrial markets. For more information, please visit ON Semiconductor’s website at https://www.onsemi.com.

# # #

ON Semiconductor and the ON Semiconductor logo are registered trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the company references its website in this news release, such information on the website is not to be incorporated herein.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.