ON Semiconductor Expands Computing Power Management Portfolio to Include Power Solutions for Notebook Applications

Share

NCP5214 DDR memory power controller integrates VDDQ and VTT termination voltage to deliver superior light load efficiency, extend battery life and simplify overall design

Intel Developer Forum (IDF) - Taipei, Taiwan – April 11, 2005 – A leading global supplier of innovative power management solutions, ON Semiconductor (Nasdaq: ONNN) today announced the expansion of its power computing portfolio with the introduction of the NCP5214. This new DDR memory power controllers integrate both VDDQ and VTT termination voltages to deliver superior system efficiency and extend battery life for notebook applications.

The integration of two voltage outputs in the new NCP5214 works to simplify overall motherboard design and save valuable space in compact portable computers. The VDDQ voltage is supplied by a high efficiency, synchronous, pulse width modulation (PWM) controller that drives two external N-channel MOSFETs. The VTT termination voltage is supplied by a linear regulator which is set to track one half of the VDDQ voltage. The VTT regulator is specified at a robust source/sink capability of 2.4 amps (A) peak.

While competitive devices offer a light load efficiency of 87 percent below 1 A, the NCP5214 performs at greater than 92 percent efficiency. The excellent light-load efficiency of these devices - paired with a shutdown current of less than 5 microamps - helps extend battery life critical in portable computing. Protection features that include VDDQ-output over-voltage protection, input under-voltage protection, thermal shutdown, and soft start circuitry and short circuit protection for both regulators all help to create a robust solution.

“The NCP5214 is the first of several power products for notebook computing that ON Semiconductor plans to introduce,” said Michael Stapleton, ON Semiconductor Director of Analog Computing Products. “All the notebook solutions under development address needs identified by computer manufacturing customers and draw upon ON Semiconductor’s proven technical expertise in the areas of desktop CPU, DDR memory, and system-wide power management, advanced integration platforms and product packaging.”

Package and Pricing
The NCP5214 will be offered in a DFN-22 leadless package and priced at $1.34 per unit in 1,000-unit quantities. Advanced engineering samples are currently available. For more information or to inquire about samples contact Andy Buk in Hong Kong at andy.buk@onsemi.com or Rebecca Chen in Taiwan at Rebecca.chen@onsemi.com.

About ON Semiconductor
With its global logistics network and strong portfolio of power semiconductor devices, ON Semiconductor (Nasdaq: ONNN) is a preferred supplier of power solutions to engineers, purchasing professionals, distributors and contract manufacturers in the computer, cell phone, portable devices, automotive and industrial markets. For more information, please visit ON Semiconductor’s website at https://www.onsemi.com.

# # #

ON Semiconductor and the ON Semiconductor logo are registered trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the company references its website in this news release, such information on the website is not to be incorporated herein.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.