ON Semiconductor Drives Power Efficiency and Protection in Portable and Consumer Electronics with New High Performance Devices

Electronica – MUNICH, Germany – Nov. 12, 2012 –

Share

Comprehensive portfolio offers highly integrated, feature-rich, lower power products developed specifically for battery-powered, noise-sensitive, space-constrained designs











Electronica – MUNICH, Germany – Nov. 12, 2012 – ON Semiconductor (Nasdaq: ONNN), driving innovation in energy efficiency, continues to enable better power conservation in a wide range of portable and consumer electronics with an expanding portfolio of highly integrated, feature-rich, low power solutions for portable and consumer electronics.

Electronica 2012 – New Portable and Consumer Product Launches

ON Semiconductor debuts two new single-channel power MOSFETs for low voltage drive switching at this year’s Electronica tradeshow and conference. The new MCH3383 P-channel MOSFET has a drain-to-source voltage (VDSS) of 12 volts (V) and a drain current (ID) of 3.5 amperes (A) with an on-state resistance (RDS(ON)) of 69 milliohms (mΩ), while the MCH3484 N-channel MOSFET has a VDSS of 20 V, an ID of 4.5 A and an RDS(ON) of 330 mΩ. These devices are highly suited to use in IC recorders and smartphones.

The NCP4545, NCP45520/21, and NCP45524/25 are also being introduced at the event, are new members of ON Semiconductor’s ecoSWITCH family of highly compact, advanced load management solutions for efficient power domain switching. Combing control and drive functionality, these devices each have soft-start via adjustable slew rate control and integrate a low RDS(ON) power MOSFET plus a charge pump. They are suitable for notebook/tablet computers, portable medical equipment, enterprise computing systems, hot swap devices, peripheral ports, telecom and industrial equipment and various portable devices.

Additionally, the NCP333, NCP334, NCP335, NCP336, and NCP337 are newly introduced cost-effective, ultra-compact, high performance load switches. Covering a 1.2 V to 5.5 V input voltage range, these MOSFET-based devices each have a built-in output discharge path to eliminate residual voltages on the output rail. They are optimized for use in cell phones, notebook/tablet computers and digital cameras.

Lastly, the NCP702, NCP703 and NCP729 are low dropout (LDO) linear voltage regulators with a 2.0 V to 5.5 V input voltage range, ultra-low quiescent current and built-in thermal shutdown mechanism. These devices’ superior performance characteristics make them highly optimized for noise-sensitive applications, where signal integrity must be maintained, such as phase locked loops, oscillators, frequency synthesizers and low noise amplifiers. Among the end products they will prove particularly suited to inclusion in are smartphones, digital cameras, tablet computers, portable DVD/media players, wireless headsets, wifi boards and portable GPS systems, as well as portable medical equipment.

Visit ON Semiconductor at Electronica 2012, 13 – 16 November, in Hall A5, at Stand 225.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.