ON Semiconductor Continues to Make Battery-less IoT a Reality with Bluetooth® Low Energy Multi-Sensor Platform

Industry’s lowest power Bluetooth radio enables new multi-sensor solution powered entirely using solar energy.

PHOENIX, Ariz. – 10 April, 2019 – ON Semiconductor (Nasdaq: ON), driving energy efficient innovations, continues to enable battery-less and maintenance-free IoT with the introduction of its RSL10 Multi-Sensor Platform powered solely with a solar cell. This complete solution supports the development of IoT sensors using continuous solar energy harvesting to gather and communicate data through Bluetooth® Low Energy, without the need for batteries or other forms of non-renewable energy.

The powerful combination of ultra-low-power wireless communications, small form-factor solar cell and low duty cycle sensing applications makes it possible to develop and deploy totally maintenance-free IoT sensor nodes. The RSL10 Solar Cell Multi-Sensor Platform is enabled by the RSL10 SIP, a complete System-in-Package (SiP) solution featuring the RSL10 radio, integrated antenna and all passive components.

The platform combines the RSL10 SIP with a solar cell and a host of low power sensors from Bosch Sensortec, including the BME280 all-in-one environmental sensor (pressure, temperature, humidity) and the BMA400 ultra-low-power 3-axis accelerometer. Together, they will allow developers and manufacturers to create complete IoT nodes that are entirely powered through renewable energy or energy harvested from the sensor’s surroundings.

“After the success of the RSL10 Sensor Development Kit, we are thrilled to work with ON Semiconductor on a new cutting-edge sensor development platform that is entirely solar powered,” said Dr. Peter Weigand, Vice President of Marketing, Bosch Sensortec. “The BMA400 is the first real ultra-low-power accelerometer that doesn’t compromise on performance. Combined with the BME280 integrated environmental sensor, this provides a comprehensive sensing solution for IoT applications such as climate control, intrusion detection and asset tracking.”

Commenting on the release of the RSL10 Solar Cell Multi-Sensor Platform, Wiren Perera, who heads IoT at ON Semiconductor, said: “To support the growth of IoT, manufacturers are actively investigating alternative sources of energy to power their designs, helping to reduce environmental impact and lower manufacturing and maintenance costs. With this solution, established on the RSL10 Bluetooth Low Energy radio, we are proving that a battery-free and maintenance-free approach to smart sensor development is not only possible but can help manufacturers improve their designs.”

There are a growing number of IoT sensor applications where the duty cycle is low enough to support intermittent communications, allowing the energy needed to support operation to be harvested using renewable sources. The energy efficiency of the RSL10 is augmented by the highly efficient power management system and the ultra-low-power sensors implemented in the platform. Applications are expected to include smart home and building automation such as HVAC control, window/door sensors and air quality monitoring. Asset tracking including package open/close detection, shock monitoring, and temperature and humidity data logging are also possible applications.

For easy development, the platform is supplied with all design files (Gerber, schematic and BoM) and customizable source code as part of a CMSIS software package. The RSL10 Solar Cell Multi-Sensor Platform is available now from ON Semiconductor alongside a number of other energy-efficient rapid prototyping platforms for IoT, including the Energy Harvesting Bluetooth Low Energy Switch which just was just named 2018 China’s Most Competitive IoT Solution by China Electronic Magazine.

To learn more, read our blog, Continuous Battery-Free Sensing Technology or watch this video, From Battery Free Sensors to Vision: Making IoT Real.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner, and smarter world. onsemi is recognized as a Fortune 500® company and included in the S&P 500® index. Learn more about onsemi at www.onsemi.com.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.