ON Semiconductor CCD Image Sensor Expands Options for Astrophotography and Scientific Imaging

November 17, 2015

KAF-16200 brings high resolution and low noise to demanding applied imaging applications















Full Frame CCD Image Sensor KAF-16200.PHOENIX, AZ – Nov. 17, 2015 – ON Semiconductor (Nasdaq: ON ), driving energy efficient innovations, is advancing image capture for demanding astrophotography and scientific imaging applications with availability of a new 16.2 megapixel (MP) charge-coupled device (CCD) image sensor.

The new KAF-16200 CCD image sensor leverages the advanced design and manufacturing capabilities of ON Semiconductor to enable image capture of the highest quality. The device’s Full Frame CCD architecture provides best in class image uniformity and dark current, and the use of 6.0 micrometer (µm) pixels with a transparent gate electrode provides high sensitivity, high dynamic range, and integrated overexposure protection. Together, these allow the KAF-16200 to provide exceptional imagery and detail in an APS-H (34.6 mm diagonal) optical format.

“This new image sensor targets opportunities directly identified by our camera manufacturing customers,” said Herb Erhardt, Vice President and GM, Industrial and Security Division, Image Sensor Group at ON Semiconductor, “The KAF-16200 provides a 2x increase in resolution compared to our current device addressing this segment, without sacrificing the CCD-level image quality required for these applications. This is another example of ON Semiconductor’s ability to leverage a broad technology base to provide the highest quality image sensor devices regardless of the underlying technology.”

The KAF-16200 is available in a RoHS-compliant CERDIP package, and is available in both monochrome and color configurations.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner and smarter world. onsemi is recognized as a Fortune 500® company and included in the Nasdaq-100 Index® and S&P 500® index. Learn more about onsemi at www.onsemi.com.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.
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
Please select one of the press categories.

Select Language:

Please select at least one of the languages.
Please select at least one of the languages.
Please select at least one of the languages.

*I agree that the information that I provide will be used in accordance with the terms of the onsemi Privacy Policy