ON Semiconductor and Hexius Semiconductor Expand Scope of Analog Functionality for Next Generation Mixed Signal ASICs

PHOENIX, Ariz. - Jan9, 2017 -

Share

New intellectual property offering will accelerate time to market and reduce development-cycle risk

PHOENIX, Ariz. - Jan9, 2017 - ON Semiconductor (Nasdaq: ON), driving energy efficient innovations, has announced a collaboration with Hexius Semiconductor to qualify several of their analog intellectual property (IP) blocks in its popular ONC18 0.18 µm CMOS process.This enables ON Semiconductor to better serve its customers with proven analog IP that can ultimately reduce design cycles and time-to-market. The eight initial designs resulting from this collaboration include a variety of analog-to-digital converters, digital-to-analog converters, voltage references and current references. There is provision, if needed, for the designs to be custom-tailored to match particular application demands. Further data converter and PLL designs are currently being developed for introduction later this year.

ON Semiconductor’s ONC18 process relies on a 0.18 micrometer (µm) CMOS architecture and due to its high voltage capabilities is extremely well suited to automotive, industrial, military and medical deployment. By having access to an expansive portfolio of qualified IP that supports this process, customers will be able to benefit from ASIC implementations that are highly optimized for their specific requirements, without needing to allocate too much of their own engineering resources to the task. As a result, much quicker design cycles, reduced risk of re-spins and lower associated costs can all be realized.

“The mixed signal ASIC market continues to grow as systems need to utilize the real-word data that is captured by sensors and user interface,” states Rocke Acree, Director of the Custom Foundry business unit at ON Semiconductor. “OEMs are looking to integrate more effective proprietary designs, rather than relying on standard off-the-shelf components. Through this, performance levels can be enhanced, board space saved and unit costs significantly lowered. By working together, ON Semiconductor and Hexius Semiconductor are delivering qualified analog IP needed to facilitate this migration and enabling a new era of mixed signal design.”

“Through the combination of the respective skill sets that our two companies possess, we are in a position to supply the industry with qualified analog IP macrocells on superior semiconductor processes that will deliver clear performance and logistical advantages. This will allow OEMs to respond more quickly to market opportunities that they have identified by taking products from the concept phase right through to full commercial production in the shortest possible time,” adds Chris Cavanagh, CEO at Hexius Semiconductor.

Visit our External Intellectual Property page for more information.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.