ON Semiconductor Demonstrates Low-Light Enabled Fast Auto Focus Technology

Mobile World Congress (MWC) – Barcelona, Spain – Feb. 26, 2015 -

Share

Innovative CMOS image sensor pixel technology accelerates auto focus performance in smartphone applications while operating in challenging low-light conditions















Mobile World Congress (MWC) – Barcelona, Spain – Feb. 26, 2015 - ON Semiconductor (Nasdaq: ONNN), driving energy efficient innovations, has successfully demonstrated its second generation Phase Detect Auto Focus (PDAF) technology featuring a unique pixel micro-lens technology that enables fast focus at 25 Lux light levels. This unique technology has been successfully implemented on a 13 megapixel (MP) test chip with 1.1 micron (µm) pixels and will be utilized in a new product introduction for mobile end-market customers later this year.

Traditional smartphone autofocus (AF) algorithms use a contrast detection measurement and multiple frames to adjust the lens focus. This trial-and-error method can take over 1.2 seconds to find focus in an image. ON Semiconductor’s PDAF technology uses two pixels to measure phase information from the target image. This phase information is then used to calculate the direction and the amount the lens needs to move to focus in less than 0.3 seconds, depending on focus actuator speed. Furthermore, ON Semiconductor has implemented a unique pixel micro-lens structure which maintains sensitivity in the PDAF pixels and ensures enough light is captured for PDAF to perform in low-light conditions as low as 25 Lux (similar to a dimly lit room). Competing technologies on the market employ methods that compromise pixel sensitivity and low light auto focus performance.

“ON Semiconductor’s PDAF technology is the result of innovations in both pixel and optical stack design,” said Shung Chieh, vice president, Mobile and Consumer Division for ON Semiconductor. “The outcome is a reduction of auto focus time by nearly a factor of four and delivers a great experience to the mobile device user. The leading low-light capability of our technology enables smartphone manufacturers to deliver a fast AF experience across all light levels to their customers.”

ON Semiconductor will be demonstrating its latest image sensor technology and products at Mobile World Congress (MWC) 2015 in Barcelona, Spain, from March 2-5. To schedule a private tour of the company’s live image sensor demonstrations please contact your ON Semiconductor sales representative.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.