ON Semiconductor Introduces Rectifier CD-ROM with Parametric Search Features

Share

Phoenix, AZ - November 9, 1999 - ON Semiconductor today announced the development of a new searchable CD-ROM for its extensive portfolio of Schottky, Ultrafast, Fast Recovery and Standard Recovery rectifiers. The CD-ROM is designed to allow engineers to quickly and effortlessly select the exact device that best fits their application. The CD-ROM offers a complete collection of ON Semiconductor's rectifier information in one location.

The rectifier CD-ROM contains a selector guide, data sheets, device cross references and application notes in pdf format. Also included are device reliability data, packaging and thermal specifications as well as SPICE and SABER models.

The selector guide provided in the rectifier CD-ROM is complete with pull down menus that offer device selections by both package and technology. A picture of the devices simplifies the selection process and the data sheets can be viewed and printed directly from the selector guide screen. Equipped with unique search capabilities, the CD-ROM device searches can be conducted based on the following parameters: IO, VRRM, IFSM, VF, TRR and package. The rectifier CD-ROM is user friendly and easy to use.

Both the selector guide and the search function included in the CD-ROM, provide the user the capability to print a report containing the results of his search. A library of rectifier and rectifier related application notes is available in pdf format. In the applications notes section, there is a complete rectifier handbook which contains everything a designer may want to know about rectifiers. There is also a brochure on Thermal Modeling and Management of Discrete Surface Mount Packages in pdf format.

For easy access to the ON Semiconductor web site, a selection button is incorporated into the menu. It enables the user to quickly access information on other ON Semiconductor discrete, analog, power and logic products and requires an Internet connection to use. This rectifier CD-ROM is compatible with both Windows 99 and Macintosh platforms and includes a downloadable Adobe Acrobat Reader for viewing the pdf files.

To order your free rectifier CD-ROM, simply request RECTFRCDROM/D by contacting ON Semiconductor via one of the following methods:

North America:
Literature Distribution Center for ON Semiconductor
P.O. Box 5163, Denver, Colorado 80217 USA
Phone: 303 675-2175; Toll Free USA/Canada: 800 344-3860
Fax: 303 675-2176; Toll Free USA/Canada: 800 344-3867
Email: ONlit@hibbertco.com

Europe
German:
Phone: 303 308-7140
Email: ONlit-german@hibbertco.com

French:
Phone: 303 308-7141
Email: ONlit-french@hibbertco.com

English:
Phone: 303 308-7142
Email: ONlit@hibbertco.com

Asia/Pacific:
LDC for ON Semiconductor - Asia
Phone: 303 675-2121; Toll Free from Hong Kong: 800 4422-3781
Email: ONlit-asia@hibbertco.com

Japan:
ON Semiconductor, Japan Customer Focus Center
4-32-1 Nishi-Gotanda, Shinagawa-ku, Tokyo, Japan 141-8549
Phone: 81 3-5487-8345
Email: r14153@onsemi.com

About ON Semiconductor
ON Semiconductor, formerly a division of Motorola, is the world's leading supplier of analog, logic and discrete semiconductor components with shipments of 15 billion units in 1998 totaling $1.5 billion in sales. These power and interface products are an integral part of electronics that provide the security, convenience and entertainment in today's world. ON Semiconductor is the tradename of SCG Holding Corporation.

For more information:

Yinka Massally
Public Relations Manager
ON Semiconductor
602-244-6398
Linda Capcara
Account Director
Brodeur Worldwide
602-954-0044
Dave Hollander
Marketing Communications Manager
Brodeur Worldwide
602-244-5971

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.