Share

Fully protected drivers control numerous loads while providing true design flexibility and advanced performance, features, fault monitoring and reporting capabilities

CONVERGENCE – DETROIT, MI – Oct. 16, 2006 – ON Semiconductor (Nasdaq: ONNN), a global leader in power management products, today introduced two new drivers specifically designed for robust automotive and industrial applications. The NCV7513 is a programmable six channel low−side MOSFET pre−driver designed to control a variety of load types. The NCV7708 is a hex half-bridge driver specifically designed to drive power system motors and loads.

“These new drivers from ON Semiconductor represent the ultimate in design flexibility,” said Jim Alvernaz, director of ON Semiconductor’s Automotive Power Products Division. “From lamps to relays and motors to LEDs, these devices offer a cost effective solution for driving a wide variety of loads. They also feature the communications and diagnostics capabilities needed in today’s safety conscious vehicles.”

The NCV7513 is a fully protected six channel low-side Hex Pre-Driver designed for a wide variety of loads, including engine control, memory seats and LED headlamps. This device is the newest member of a growing family of FLEXMOS™ automotive-grade products for driving logic level MOSFETs. The NCV7513 is controllable by a combination of Serial Peripheral Interface (SPI) and parallel inputs. With 3.3 volt (V) and 5.0 V compatible inputs, it is ideal for use with the newer microcontrollers. Each of the six channels independently monitors its external MOSFETs for fault conditions. It features programmable fault management modes and allows power−limiting pulse width modulation (PWM) operation. The fault information for each channel is uniquely captured by fault type.

The NCV7513 is available in a 32-pin LQFP package and priced at $0.82 per unit in 10,000 unit quantities.

The NCV7708 is a fully protected Hex Half Bridge Driver and the newest member of a family of multi-channel drivers. The device features six independent high side and six independent low side drivers that are also configurable as H-bridge drivers. The NCV7708 is controlled via SPI up to 5 megahertz (MHz). It offers advanced fault reporting and protection features, and is compliant with 5 V and 3.3 V systems.

“What makes the NCV7708 particularly versatile is the fact that it can drive high side loads, low side loads and motors,” said Alvernaz. “At Convergence, ON Semiconductor will run a live demonstration of this device driving automotive mirrors, puddle lamps, and HVAC blender motors.”

The NCV7708 is offered in a 28-pin SOIC thermally enhanced fused lead package and priced at $1.25 per unit in 10,000 unit quantities.

For additional technical information visit www.onsemi.com or contact Richard White at richard.white@onsemi.com.

About ON Semiconductor
With its global logistics network and strong portfolio of power semiconductor devices, ON Semiconductor (Nasdaq: ONNN) is a preferred supplier of power solutions to engineers, purchasing professionals, distributors and contract manufacturers in the computer, cell phone, portable devices, automotive and industrial markets. For more information, please visit ON Semiconductor’s website at https://www.onsemi.comhttps://www.onsemi.com.

# # #

ON Semiconductor and the ON Semiconductor logo are registered trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the company references its Web site in this news release, such information on the Web site is not to be incorporated herein.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. With a highly differentiated and innovative product portfolio, onsemi creates intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way in creating a safer, cleaner, and smarter world.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.