May 18, 2020

Share:

Automotive lighting continues to be one of the most important parts of a vehicle, and innovation in this area continues. Automotive manufacturers are now adding new colors and functionality to classic lighting systems in order to provide enhanced aesthetic appeal and customization, as well as to improve safety. As the automotive industry evolves towards fully autonomous vehicles (AV), the function of lighting is becoming even more vital, enabling safety features for the driver, pedestrian and other vehicles on the road.

In absence of the driver, or in the event that the driver is not paying attention to the road, there is a need for the car to replace eye-contact and use lighting to communicates with other users and/or vehicles. That communication goes from providing the vehicle status: parked, waiting or driving, to providing safety-related information. If you are to look at the vehicle head-on, this might include giving clearance to pedestrians at a pedestrian crossing; while in the rear, it could give a warning to following cars that crossing pedestrians are ahead. (The car industry is in the process of selecting a new color for this AV-related messaging.) Other recent enhancements include custom tail light appearance and greeting (welcome and goodbye) animations.

To learn more about the new evaluation board and see it in action, watch below!


To support automotive design engineers in developing these new applications, ON Semiconductor has released the new SECO-NCV7685RGB-EVB platform, a cost-efficient lighting solution with Bluetooth Low Energy (BLE) remote control functionality. The new platform includes LED drivers, Low Dropout regulators (LDOs) and wireless functionality. It provides a reference design targeting next-generation intelligent tail lighting or interior lighting applications. A mobile app allows users to set the RGB LED color and intensity and show customized information and animation.


The new evaluation board includes 4 NCV7685 LED drivers, each capable of driving 4 RGB LEDs to be driven with up to 60 mA per channel - as each NCV7685 integrates up to twelve current sources with high resolution dimming. With the 16-bit I/O port expander PCA9655E and floating address setting in firmware, NCV7685 is assigned defined addresses instead of being locked into one time programmable (OTP) registers at power on, which provides convenience for aftermarket maintenance. The NCV8170 LDO regulator and the NCV891330 dual mode regulators power the NCV7685 and the LED string in a cost-efficient way.


With the addition of the RSL10 SIP, the connectivity module provides low-power LED wireless control options, allowing the user to program animation effects via a mobile application. The RSL10 is a Bluetooth 5, multi-protocol radio System on Chip (SoC) bringing ultra-low-power BLE to wireless applications and offering the industry’s lowest power consumption.

Be sure to subscribe to our blog and follow us on social media to receive the latest updates on our technologies, solutions and company news!

Twitter | Facebook | LinkedIn | Instagram | YouTube

Featured

Interior Lighting

We offer a variety of discrete and monolithic solutions for a full range of applications. These include simple solutions such as our two terminal constant current regulators (CCRs), which are economical, robust devices that provide an effective solution for regulating current in cost sensitive automotive LED applications. More complex solutions include LIN RGB LED drivers, that combine a LIN transceiver with a RGB LED driver and memory, providing a single-chip RGB driver intended to monitor dedicated multicolor LED applications.

Exterior Lighting

Styling and safety are enhanced with the addition LED exterior lighting systems. onsemi provides a variety of discrete, linear programmable constant current devices designed for regulation and control of LED based lighting systems. These linear current regulator/controllers are able to drive rear combination lamps, day time running lights, and turn signals. They allow for two programmed levels for Stop and Tail illumination, and also slew rate control to eliminate EMI concerns.

LED Lighting

Modern automotive lighting offer more functionalities than just providing light. Working in tandem with advanced driver assistance system (ADAS), they provide dynamic light distribution making the night drives safer and less tiring for the drivers. It is expected that vehicles will include LED (Light Emitting Diodes) light sources in more and more functions. LED drivers control LEDs while increasing efficiency by implementing more modern topologies e.g., synchronous switching. With improvements in LED technology, more light output can be achieved more efficiently.

Automotive lighting includes devices mounted in front, rear, sides and interior of the vehicle. LEDs consume significantly less power while providing brighter and more focused illumination. This efficiency not only reduces the load on the vehicle’s electrical system but also contributes to better fuel economy. Additionally, LEDs have a much longer lifespan, lasting more than 10,000 hours, which means fewer replacements and lower maintenance costs for vehicle owners.