onsemi to Show Best-In-Class Image Sensing at VISION

Stuttgart, Germany – Sept. 29, 2022 – onsemi

Share

Live demonstrations will highlight the latest image sensing solutions for multiple industry sectors

Stuttgart, Germany – Sept. 29, 2022 – onsemi (Nasdaq: ON), a leader in intelligent power and sensing technologies, will showcase its latest image sensing technology at VISION – the world’s leading trade fair for machine vision – at booth 10G30.

Handheld barcode readers need to be fast, reliable and have good battery life to meet increasing expectations for worker productivity from retail stores to e-commerce warehouses. onsemi will demonstrate a barcode reader solution featuring a new 1/8” VGA CMOS digital image sensor that is four times better than the global shutter efficiency of the previous generation of onsemi’s VGA image sensors. The small size and ultra-low power consumption allow deployment in extremely compact vision systems. The new sensor is fully supported by the AP1302 co-processor and other industry-leading image signal processors over a single lane MIPI interface, delivering full resolution image data at 120 frames per second (fps).

onsemi will also showcase a high-resolution image sensor focused on machine vision applications. This 1/2" 20MP image sensor has many functional features using proprietary technologies that deliver exceptional image quality across all operating conditions and delivers high performance with a very low power footprint. For applications where power consumption and/or bandwidth are a concern, the sensor can be configured to output a variety of low-resolution image formats.

In collaboration with Leopard Imaging, onsemi will demonstrate a Vision Guided Robotics solution that addresses depth accuracy with the popular AR0234CS image sensor. This 1/2.6” 2.3MP image sensor operates off global shutter technology, is capable of delivering 120 fps at full resolution and a pair is highly suited to create stereoscopic vision required for depth measurements. The solution showcases 2D/3D imaging output running on the popular NVIDIA® Jetson™ platform and provides industry-leading depth accuracy. Additionally, the platform demonstrates a monocular camera solution running in parallel to deliver intelligent vision solutions as in smart label identification, OCR & bar codes and more.

VISION visitors will also be able to see the onsemi XGS family of CMOS image sensors, particularly the X-Cube reference design and X-Celerator FPGA development platform, based on the XGS 5000 (5.3 MP 2592 x 2048 px), XGS 16000 (16.0 MP 4000 x 4000 px) and the flagship XGS 45000 (44.7 MP 8192 x 5460 px), able to run at 8K video at 60 fps. These image sensors can deliver multiple resolutions and frame rates with 12-bit resolution. The family of advanced devices is built upon an innovative 3.2 m global shutter pixel, enabling XGS devices to offer outstanding image quality and uniformity – even at high resolutions.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner, and smarter world. onsemi is recognized as a Fortune 500® company and included in the S&P 500® index. Learn more about onsemi at www.onsemi.com.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.

If you are a member of the press and are interested in receiving onsemi press releases via email, please complete the form below.

* Full Name

* Email

* Media you represent

* Press Category

*Required fields

Choose your prefered language. You can choose more than one.