onsemi Redefines Brushless DC Motor Control with ecoSpin Family

With an embedded gate driver and a microcontroller engine, ecoSpin™ BLDC motor control solutions provide reliable, scalable operation up to 600V

PHOENIX – Oct. 27, 2022 – onsemi (Nasdaq: ON), a leader in intelligent power and sensing technologies, today introduced its new ecoSpin™ family of brushless DC (BLDC) motor controllers. By combining the control and driver functions in a complete system-in-package (SiP) solution, onsemi simplifies the development of high-voltage motor control systems in applications such as HVAC, refrigeration and robotics.

The first member of the ecoSpin family to be launched is the ECS640A, a three-phase brushless DC (BLDC) motor controller designed for reliable high-voltage operation up to 600 V. The small-form-factor ECS640A features a trusted gate driver, Arm® Cortex-M0+ microcontroller, three sense amplifiers, three bootstrap diodes and can support either sensored or sensorless motor control architectures.

“The highly integrated solution reduces time to market by eliminating the need for design cycles on applications, simplifying solution reuse when scaling BLDC motor power level requirements,” said Michel De Mey, vice president of the Industrial Solutions Division, onsemi. “Reliability is improved by replacing many of the larger, more complex devices, while at the same time shrinking the PCB routing area by approximately 20% compared to a discrete implementation, to deliver an overall compact solution.”

The integration in a single IC package (10 by 13 mm) redefines BLDC motor control performance by optimizing power stage placement and reducing noise. This allows rapid reuse in alternative platforms by simply changing the discrete power devices and updating the software. The reduction in BOM simplifies sourcing challenges stemming from having many different discrete devices.

To optimize performance, the ECS640A supports traditional motor control techniques including trapezoidal and vector control. Advanced commutation algorithms are available on the Cortex M0 platform. These techniques allow for improved control over the motor’s flux and torque over a wide speed range, with as much as a three to five percent improvement in power efficiency.

With a compact system design and user-friendly tools to accelerate the design process, the ECS640A brings new levels of ease-of-use to BLDC motor control. The ECS640A is available now through onsemi sales support and authorized distributors.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner, and smarter world. onsemi is recognized as a Fortune 500® company and included in the S&P 500® index. Learn more about onsemi at www.onsemi.com.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.