September 16, 2026

Share:

onsemi site entrance

Company outlines a $213 billion market opportunity as power becomes the foundational technology layer from infrastructure to physical applications

Scottsdale, Ariz. — September 16, 2026 — onsemi (NASDAQ: ON) today outlined its long-term growth strategy to lead one of the largest and most consequential technology shifts of the next decade by solving the growing power constraints limiting the advancement of AI, electrification and automation. As these markets converge around common technology requirements, onsemi is leveraging its differentiated portfolio across power and sensing to address a $213 billion market opportunity and solve the needs of some of the most important technology trends shaping the global economy.

“Every transformational technology eventually encounters a physical constraint. As AI, electrification and automation continue to scale, power density is emerging as one of the defining engineering challenges of this decade,” said Hassane El-Khoury, President and CEO of onsemi. “The companies that lead in the next era of innovation will be those that can deliver more energy while consuming less space. As that challenge becomes more urgent, power has become a foundational technology layer that will help shape the pace of innovation, economic growth and global competitiveness. We have spent years building deep expertise and a broad portfolio across power and sensing to help customers solve this challenge and enable the next generation of intelligent machines.”

Watch the keynotes here: 2026 Investor Day: Accelerating the Future

Unlocking a $213 Billion Opportunity

onsemi sees a $213 billion total addressable market by 2030 spanning automotive, industrial, AI data centers and emerging applications. Although these markets are often viewed separately, they increasingly rely on the same underlying capabilities: efficient power conversion, perception of the physical world, and edge intelligence and connectivity.  

This convergence allows onsemi to deploy common technology platforms across multiple end markets. A high-voltage technology developed for automotive electrification, for example, can also support industrial energy systems and AI data centers. Advances in sensing and connectivity can extend across vehicles, factories, robotics, medical systems and other autonomous applications.

The company expects this platform-based model to increase the revenue potential of its core technologies by moving from individual components to higher-value solutions and system architectures that address a larger share of each customer's design requirements. Through this approach, onsemi can generate greater leverage from its R&D investments, reduce dependence on any single end market or technology cycle, and grow faster than the markets it serves.

“Throughout history, foundational technologies have created outsized value because they enable everything built above them,” El-Khoury said. “Power has become the common denominator across these end markets. For onsemi, that creates opportunities to innovate beyond any market trend, with multiple paths to expand content, gain share and capture more value.”

Solving the Next Challenge: Power Density

Capturing this opportunity requires addressing a growing constraint facing AI infrastructure and other intelligent systems – power density – or the ability to deliver greater performance and capability using less energy and less physical space. Next-generation systems must use available energy more productively while generating less heat, occupying less space and maintaining reliability at scale.

Increasing power density requires electrical, thermal, mechanical and physical performance to be optimized simultaneously. Increasing power typically generates more heat, while reducing system size can make that heat more difficult to remove. Improving efficiency may require new materials, device architectures and integration methods. Historically, these trade-offs forced system designers to make compromises among power, size, cost and thermal performance.

As these challenges become more complex, value increasingly shifts to companies that can optimize across the entire system. onsemi has expanded beyond traditional power semiconductors to build capabilities spanning technologies, products, solutions and systems. onsemi highlighted three technology platforms that will shape the next generation of intelligent systems and drive long-term growth across its key end markets:

High-Voltage Technologies: The Device Layer 

onsemi's high-voltage portfolio spans silicon, silicon carbide and gallium nitride, giving customers a range of options to optimize performance, efficiency, power density and cost. The portfolio includes vertical gallium nitride (vGaN), a differentiated technology, exclusive to onsemi, designed for next-generation high-voltage applications that can increase efficiency, improve switching performance and reduce system size where conventional power technologies are reaching their limits.

Treo: The Intelligence Layer

Modern systems must do more than convert power. They must monitor operating conditions, communicate across the system, respond to changing loads and protect critical functions in real-time. The Treo platform’s high precision analog, high density digital and high voltage capabilities, enable systems to become more precise, adaptive and autonomous. This allows onsemi to add these capabilities around the power device, increasing the functionality and value within a customer’s system.

Embedded Power Platform (EPP): The Integration Layer

EPP reimagines the package from passive housing into an active contributor to system performance. By using the silicon wafer itself as the package, EPP enables the seamless integration and interconnection of silicon, silicon carbide (SiC) and gallium nitride (GaN) technologies within a highly integrated wafer-level architecture. Multiple devices, including FETs, drivers and controllers, can be embedded together in a single package and co-optimized for electrical, thermal and mechanical performance. This enables complete power-system co-design, allowing electrical, thermal and mechanical characteristics to be evaluated and optimized together from day one. The result is higher power density, improved system performance, reduced development complexity and faster time-to-market.

onsemi Embedded Power Platform Wafer
onsemi Embedded Power Platform Chip

As customers increasingly seek complete solutions rather than individual components, onsemi solves a larger portion of the customer’s challenge by reducing design complexity and accelerating development across automotive, industrial, AI data center and physical AI applications. With this focus on the entire system-level solution, onsemi creates a competitive advantage that is difficult to replicate through individual components alone.

Beyond the Data Center: AI's Next Frontier is the Physical World

While today's AI investments are largely focused on building the infrastructure needed to train and run increasingly sophisticated models, the next phase of growth will occur at the edge, where intelligence moves beyond the data center into machines that interact directly with the physical world.

These physical AI systems must sense, decide, act and adapt safely in real-world environments, in real-time. Whether deployed in a robot, vehicle, factory, medical system or autonomous platform, each system requires four capabilities to operate together:

  • Power to provide the energy foundation that enables intelligent systems to operate
  • Sense to perceive and understand the physical environment
  • Control to execute decisions through precise real-world actions
  • Connected Compute to process, share and continuously adapt information at the edge

As this transition happens, many of these same technologies onsemi developed for automotive and industrial applications can be applied to this emerging market. onsemi's ability to combine these capabilities through system-level co-design and optimize performance across the full stack, positions it to deliver differentiated solutions and capture a larger share of the value created by physical AI.

“The most attractive opportunities of the next decade are emerging as markets converge around the same technologies,” El-Khoury said. “The ability to efficiently deliver power, sense the environment and enable intelligent decision-making will define the next generation of intelligent machines. Our differentiated technology platforms enable us to solve power density across the device, intelligence and integration layers in a way no other semiconductor company can, positioning us to expand our content and grow as AI moves from infrastructure into the physical world.”

More Information:

About Embedded Power Platform:

Caution Regarding Forward-Looking Statements

This press release includes “forward-looking statements,” as that term is defined in Section 27A of the U.S. Securities Act of 1933, as amended, and Section 21E of the U.S. Securities Exchange Act of 1934, as amended. All statements, other than statements of historical facts, included or incorporated in this press release could be deemed forward-looking statements, particularly statements about onsemi’s long term growth strategy; forecasts about the pace, scale and direction of technological change and its impact on onsemi’s total addressable market opportunity; statements about onsemi’s ability to capitalize on such an opportunity; and the potential impact of each of the foregoing on onsemi’s operating results and financial condition. Forward-looking statements are often characterized by the use of words such as “believes,” “estimates,” “sees,” “expects,” “projects,” “may,” “will,” “intends,” “plans,” “anticipates,” “targets,” “should,” “would” or similar expressions or by discussions of strategy, plans, expectations, projections or intentions. All forward-looking statements in this document are made based on onsemi’s current expectations, forecasts, estimates and assumptions and involve risks, uncertainties and other factors that could cause results or events to differ materially from those expressed in the forward-looking statements. Certain factors that could affect onsemi’s future results or events are described under Part I, Item 1A “Risk Factors” in the 2025 Annual Report on Form 10-K filed with the Securities and Exchange Commission (“SEC”) on February 9, 2026 (the “2025 Form 10-K”) and from time to time in onsemi’s other SEC reports. Readers are cautioned not to place undue reliance on forward-looking statements. onsemi assumes no obligation to update such information, which speaks only as of the date made, except as may be required by law.

Investing in onsemi’s securities involves a high degree of risk and uncertainty, and you should carefully consider the trends, risks and uncertainties described in this press release, onsemi’s 2025 Form 10-K and other reports filed with or furnished to the SEC before making any investment decision with respect to onsemi’s securities. If any of these trends, risks or uncertainties actually occurs or continues, onsemi’s business, financial condition or operating results could be materially adversely affected, the trading price of onsemi’s securities could decline, and you could lose all or part of your investment. All forward-looking statements attributable to onsemi or persons acting on onsemi’s behalf are expressly qualified in their entirety by this cautionary statement.