ON Semiconductor's SiC Diodes Offer Higher Efficiency, Power Density and Lower System Costs

February 28, 2018

650 V silicon carbide Schottky diodes feature superior switching performance and higher reliability

APEC 2018 – Booth #601 – SAN ANTONIO, TX – February 28, 2018 - ON Semiconductor (Nasdaq: ON), driving energy efficient innovations, has extended its SiC diode portfolio by introducing its newest family of 650 V silicon carbide (SiC) Schottky diodes. The diodes' cutting edge, silicon carbide technology provides higher switching capabilities with lower power losses and effortless paralleling of devices.

ON Semiconductor's newly released family of 650 V SiC diodes includes surface mount and through hole packages ranging from 6 Amperes to 50 Amperes (A). All of the diodes provide zero reverse recovery, low forward voltage, temperature independent current stability, high surge capacity and positive temperature coefficient.

The new diodes are aimed at engineers designing PFC and boost converters for various applications including solar PV inverters, EV/HEV chargers, telecom power and data center power supplies while facing challenges to deliver smaller footprints at higher efficiencies.

The 650 V devices offer the combined system benefits of higher efficiency, higher power density, smaller footprints and enhanced reliability. They exhibit a reduced power loss due to the inherent low forward voltage (VF) and no reverse recovery charge of SiC diodes, and hence improved efficiency. The faster recovery of SiC diodes allows for higher switching speeds and therefore reduces the size of magnetics and other passive components, enabling greater power density and smaller overall circuit designs. In addition, the SiC diodes can withstand higher surge currents and deliver stability over their -55 to +175 degrees C operating temperature range.

ON Semiconductor's SiC Schottky diodes feature a unique, patented termination structure that reinforces reliability and enhances stability and ruggedness. Additionally, the diodes offer higher avalanche energy, the industry's highest unclamped inductive switching (UIS) capability and lowest leakage currents.

"ON Semiconductor's new 650 V family of SiC diodes complement the company's existing 1200 V SiC devices, bringing a broader product range to our customers," said Simon Keeton, Senior Vice President and General Manager, MOSFET Business Unit, ON Semiconductor. "Utilizing the unique characteristics of wide band gap materials, SiC technology offers tangible benefits over silicon, and their robust construction provides a dependable solution in applications in challenging environments. Our customers will benefit from simplified, better performing, smaller footprint designs as a result of these new devices."

Packaging and Pricing

The 650 V SiC diode devices are offered in DPAK, TO-220, and TO-247 packages and priced from $1.30 to $14.39 per unit in 1,000 unit quantities.

Join ON Semiconductor at APEC (booth #601), where visitors can see a live demonstration of its SiC MOSFET and diodes, showing how the company's latest simulation modelling techniques can accurately match real life device operation.

About onsemi

onsemi (Nasdaq: ON) is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner, and smarter world. onsemi is recognized as a Fortune 500® company and included in the S&P 500® index. Learn more about onsemi at www.onsemi.com.

###

onsemi and the onsemi logo are trademarks of Semiconductor Components Industries, LLC. All other brand and product names appearing in this document are registered trademarks or trademarks of their respective holders. Although the Company references its website in this news release, information on the website is not to be incorporated herein.